Skip to main content
Maksh.1
Associate III
August 10, 2021
Question

Hi, I have created a STM32 project using STM32CubeIDE , Now I need to integrate Cortex-M4 firmware with distribution on yocto.

I copied the STM32CubeIDE project into PATH: openstlinux-5.10-dunfell-mp1-21-03-31/layers/sources/m4projects-stm32mp1/Projects/STM32MP1

Added projects path in recipes-extended/m4projects/m4projects-stm32mp1.bb

But i find that file structure for examples is different from the file structure of STM32CubeIDE project

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
August 27, 2021

Hi @Maksh.1​ ,

Sorry for late reply.

Did you manage to find a solution ? Where do you stand ?

Yes, exemple may use slightly different file structure vs STM32CubeIDE generated project but what is exactly the issue in Yocto ?

Can you elaborate ? Any build log to share ?

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.