Skip to main content
NKorn.3
Visitor II
November 30, 2020
Question

Hello I'm trying to write a loadable kernel module driver. I get an error during compilation: ERROR: modpost: "platform_device_alloc" [/home/rdm/ethtest/eth-ins.ko] undefined! Do I need something to set in the Kernel Config? Helloworld works as LKM.

#include <linux/platform_device.h>

#include <linux/module.h

#include <linux/types.h>

MODULE_LICENSE("GPL");

MODULE_AUTHOR("Robert W. Oliver II");

MODULE_DESCRIPTION("A simple example Linux module.");

MODULE_VERSION("0.01");

static struct platform_device *pdev;

static int __init fake_eth_add(void)

{

  int inst_id = 0;

  pdev = platform_device_alloc("fake-eth", inst_id);

  return 0;

}

static void __exit fake_eth_put(void)

{

}

module_init(fake_eth_add);

module_exit(fake_eth_put);

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
December 2, 2020

Hi @Community member​ 

Did you refer to following wiki page ?

https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package#Modifying-2Fadding_an_external_Linux_kernel_module

Such kind of error usually come from bad installation / initialization of the SDK.

Double check your environment.

Hope it help,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.