Skip to main content
ASuha.1
Visitor II
March 30, 2021
Question

Hello, I am trying to execute a simple ADC program(12bit) in stm32mp157c using trimpot with 10K as input in cube ide. Where output changes only at the voltage level of 3.2v

While changing the value at the trimpot output values is constant(4095) and has no change as soon as when it reaches 3.2V it goes to zero. I am seeing output using uart.

​

Please assist me how to rectify it.​

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
March 30, 2021
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent