Skip to main content
Vlaty.1
Associate III
October 16, 2020
Question

Good afternoon. I tried to check your example OpanAMP_TTY_echo together with the ssh-t ttyRPMSG0 command after trying to execute the ssh-t ttyRPMSG0 command, the terminal responds Error resolving ttyRPMSG0 port 22 Temporary failure in name resolution

Good afternoon. I tried to check your example OpanAMP_TTY_echo together with the ssh-t ttyRPMSG0 command after trying to execute the ssh-t ttyRPMSG0 command, the terminal responds Error resolving ttyRPMSG0 port 22 Temporary failure in name resolution Why? What did I do wrong? Sincerely, Alexander

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
October 26, 2020

Hi @Vlaty.1​ 

Can you better explain what you are trying to achieve ?

ttyRPMSG0 is used to exchange message/data between A7 and M4.

From where did you try to connect with ssh-t ttyRPMSG0 ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Vlaty.1
Vlaty.1Author
Associate III
October 27, 2020
Good morning. Thanks for the help. But when trying to contact stm32mp157a-DK1 (), there is no communication channel again. Device on com 3, idle/busy status .Address 192.163.1.7 once green . This usually worked stably. Sincerely, Alexander. пн, 26 окт. 2020 г. в 19:23, ST Community :