Skip to main content
Jzhua
Associate III
December 9, 2019
Solved

gcnano is not install in rootfs

I built the rootfs according to the instructions at https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package, but the userspace program of gcnano is not installed in the rootfs, the / vendor directory is empty.

I need to manually install gcnano-userland- multi-binary-stm32mp_6.2.4.p4-r0.0_armhf.deb to complete the installation, where is the problem

This topic has been closed for replies.
Jzhua
JzhuaBest answer
Associate III
December 10, 2019

I think I know why,the gcnano is packaged in st-image-vendorfs-openstlinux-weston-stm32mp1.tar.xz,and i only unpackage st-image-simple-openstlinux-weston-stm32mp1-20191122051913.rootfs.tar.xz for the nfs.

so unpackage st-image-vendorfs-openstlinux-weston-stm32mp1.tar.xz into /vendor solve the issue

3 replies

Olivier GALLIEN
ST Technical Moderator
December 9, 2019

Hi @Jzhua​ 

Did you well accept EULA when setting up the Distribution ?

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Jzhua
JzhuaAuthor
Associate III
December 10, 2019

yes, I accepted with the EULA

the local.conf has ACCEPT_EULA_stm32mp1 = "1"

​