Skip to main content
NPal.2
Associate III
July 2, 2021
Solved

Force re-compile local kernel changes

Hi,

I have done certain changes to support the display in the dts files.

I have modified dts files under kernel and u-boot.

I had also added certain changes in panel-simple.c file as well.

I gave a build and forgot to make some changes. So i changed those locally and gave :

bitbake st-image-weston

But this time around upon checking i found out that latest changes i made were not compiled and a new .o was not generated. How can i make sure , that local changes are compiled by yocto build system??

This topic has been closed for replies.
Mikalaj Karhin
Mikalaj KarhinBest answer
Associate II
July 5, 2021

It looks like you are making changes to the temporary build directory.

You need to clone the u-boot and kernel source code, make changes, create patches and add them to the layer.

6 replies

Mikalaj Karhin
Associate II
July 3, 2021

Hey!

From which folder did you change dts?

NPal.2
NPal.2Author
Associate III
July 5, 2021

Hi @Mikalaj Karhin​ : I changed the driver file : drivers/gpu/drm/panel/panel-simple.c

Mikalaj Karhin
Associate II
July 5, 2021

Did you create a patch and add it to a build layer?

NPal.2
NPal.2Author
Associate III
July 5, 2021

I directly modified the file under the kernel-source folder which was downloaded. It was a local change. I did not create patch and added it to yocto .

Mikalaj Karhin
Mikalaj KarhinBest answer
Associate II
July 5, 2021

It looks like you are making changes to the temporary build directory.

You need to clone the u-boot and kernel source code, make changes, create patches and add them to the layer.

NPal.2
NPal.2Author
Associate III
July 10, 2021

THanks @Mikalaj Karhin​ for the suggestion. Will take a look this might help.