Skip to main content
JSpra
Associate III
March 29, 2021
Question

FDCAN filters not working on STM32mp157

HI,

I'm not able to get the FDCAN filter working on a STM32MP157C-DT2. I'm able to receive valid ID' with no problem, however, invalid ID's are getting through.

Would someone be kind enough to take a quick look at my setup to make sure I did not miss anything. Please see attached code.

Thank you!

This topic has been closed for replies.

2 replies

Jean-Marc S
ST Employee
May 19, 2022

Hello,

when you say "are getting through" do you mean that invalid ID's are not filtered ?

I see in your code :

if (HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_ACCEPT_IN_RX_FIFO0, FDCAN_REJECT_REMOTE, FDCAN_FILTER_REMOTE))

so FDCAN_ACCEPT_IN_RX_FIFO0 means that the invalid ID should be stored in FIFO0

is this what is happening ?

JM

Jean-Marc S
ST Employee
May 19, 2022

Just noticed the following:

you have set: hfdcan1.Init.ExtFiltersNbr = 0;

I think it should be set to 1..

JM