Associate
August 3, 2020
Question
Failed to download system image
- 8 replies
- 2765 views
Our self-made board contains emmc and lpddr3 (1GB, 32bit). The error message when downloading the image is as the attachment.
Use Uart to monitor during the download process to get the following information:
NOTICE: CPU: STM32MP157AAC Rev.Z
NOTICE: Model: Thinta TTU Board
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO PMIC version = 0x21
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.2-r1.0(debug):v2.2-dirty
NOTICE: BL2: Built : 13:36:23, Oct 22 2019
INFO: Using crypto library 'stm32_crypto_lib'
INFO: BL2: Doing platform setup
INFO: RAM: LPDDR3 8Gb 533MHz v1.45
ERROR: DDR addr bus test: can't access memory @ 0xc0000004I have tried to replace multiple boards. Can you help find the cause of the failure?