Skip to main content
Sebastian Sepulveda
Associate
November 19, 2019
Solved

Failed to build device tree generated with STM32CubeIDE 1.1.0

STM32CubeIDE: Version: 1.1.0

STM32MP1 FW Package:

I built a custom and default device tree for A7, and fails to compile because of a syntax error (same line in both cases)

| NOTE: make -j 12 HOSTCC=gcc -isystem/repo/build-openstlinuxweston-stm32mp1-m4_afe/tmp-glibc/work/stm32mp1_m4_afe-openstlinux_weston-linux-gnueabi/linux-stm32mp/4.19-r0/recipe-sysroot-native/usr/include -O2 -pipe -L/repo/build-openstlinuxweston-stm32mp1-m4_afe/tmp-glibc/work/stm32mp1_m4_afe-openstlinux_weston-linux-gnueabi/linux-stm32mp/4.19-r0/recipe-sysroot-native/usr/lib -L/repo/build-openstlinuxweston-stm32mp1-m4_afe/tmp-glibc/work/stm32mp1_m4_afe-openstlinux_weston-linux-gnueabi/linux-stm32mp/4.19-r0/recipe-sysroot-native/lib -Wl,-rpath-link,/repo/build-openstlinuxweston-stm32mp1-m4_afe/tmp-glibc/work/stm32mp1_m4_afe-openstlinux_weston-linux-gnueabi/linux-stm32mp/4.19-r0/recipe-sysroot-native/usr/lib -Wl,-rpath-link,/repo/build-openstlinuxweston-stm32mp1-m4_afe/tmp-glibc/work/stm32mp1_m4_afe-openstlinux_weston-linux-gnueabi/linux-stm32mp/4.19-r0/recipe-sysroot-native/lib -Wl,-rpath,/repo/build-openstlinuxweston-stm32mp1-m4_afe/tmp-glibc/work/stm32mp1_m4_afe-openstlinux_weston-linux-gnueabi/linux-stm32mp/4.19-r0/recipe-sysroot-native/usr/lib -Wl,-rpath,/repo/build-openstlinuxweston-stm32mp1-m4_afe/tmp-glibc/work/stm32mp1_m4_afe-openstlinux_weston-linux-gnueabi/linux-stm32mp/4.19-r0/recipe-sysroot-native/lib -Wl,-O1 HOSTCPP=gcc -E stm32mp157c-m4_afe-mx.dtb
| GEN ./Makefile
| scripts/kconfig/conf --syncconfig Kconfig
| CC scripts/mod/empty.o
| CC scripts/mod/devicetable-offsets.s
| MKELF scripts/mod/elfconfig.h
| HOSTCC scripts/mod/modpost.o
| HOSTCC scripts/mod/sumversion.o
| HOSTCC scripts/mod/file2alias.o
| HOSTLD scripts/mod/modpost
| DTC arch/arm/boot/dts/stm32mp157c-m4_afe-mx.dtb
| Error: /repo/build-openstlinuxweston-stm32mp1-m4_afe/tmp-glibc/work-shared/stm32mp1-m4_afe/kernel-source/arch/arm/boot/dts/stm32mp157c-m4_afe-mx.dts:113.23-24 syntax error
| FATAL ERROR: Unable to parse input tree
| scripts/Makefile.lib:293: recipe for target 'arch/arm/boot/dts/stm32mp157c-m4_afe-mx.dtb' failed
| make[3]: *** [arch/arm/boot/dts/stm32mp157c-m4_afe-mx.dtb] Error 1
| arch/arm/Makefile:343: recipe for target 'stm32mp157c-m4_afe-mx.dtb' failed
| make[2]: *** [stm32mp157c-m4_afe-mx.dtb] Error 2
| Makefile:146: recipe for target 'sub-make' failed
| make[1]: *** [sub-make] Error 2
| Makefile:24: recipe for target '__sub-make' failed
| make: *** [__sub-make] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /repo/build-openstlinuxweston-stm32mp1-m4_afe/tmp-glibc/work/stm32mp1_m4_afe-openstlinux_weston-linux-gnueabi/linux-stm32mp/4.19-r0/temp/log.do_compile.10586)
ERROR: Task (/repo/layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_4.19.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 695 tasks of which 614 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
 
Summary: 1 task failed:
 /repo/layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_4.19.bb:do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

Inspecting the files the error should be on

	led {
		compatible = "gpio-leds";
		blue {
			label = "heartbeat";
			gpios = <&gpiod 11 GPIO_ACTIVE_HIGH>; // This line is 113
			linux,default-trigger = "heartbeat";
			default-state = "off";
		};
	};

I tried removing that line and section, but other similar errors happen later on the code, any ideas what could be the issue ?

Regards !

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
November 20, 2019

Hi @Sebastian Sepulveda​ 

Please confirm you are using distribution package from Release Openstlinux-4.19-thud-mp1-19-10-09

Can you please share you complete dts file ?

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

3 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
November 20, 2019

Hi @Sebastian Sepulveda​ 

Please confirm you are using distribution package from Release Openstlinux-4.19-thud-mp1-19-10-09

Can you please share you complete dts file ?

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sebastian Sepulveda
Associate
November 20, 2019

Oliver,

I was using openstlinux-4.19-thud-mp1-19-02-20. I'll update to 19-10-09 and report back