Skip to main content
KNono
Associate II
July 12, 2021
Solved

Fail the Image flashing on STM32MPU157F-DK2

Hi,

​

I am trying to flash the Starter_Package to SD card in accordance with the following wiki("6.2 Image flashing"). But fail.

https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package#Image_flashing

​

Unfortunately i am a complete beginner on these tools and don't understand what is happened.

Thank you by advance for any help or advices.

​

​

error log are...

Error: failed to download Segment[0]

Error: failed to download the File

Error: Download partition 0x06 failed

Error: TSV flashing service failed

​

My environments are below,

Bord:STM32MPU157F-DK2.

Host PC: Windows10 64 bit

SD card: ADATA 16GB

​

[Full log]

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.7.0

   -------------------------------------------------------------------

​

​

​

USB speed  : High Speed (480MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

SN     : 002700363030510D32313933

FW version : 0x0110

Device ID  : 0x0500

Device name : STM32MP1

Device type : MPU

Device CPU : Cortex-A7

​

​

Start Embedded Flashing service

​

​

​

Memory Programming ...

Opening and parsing file: tf-a-stm32mp157f-dk2-usb.stm32

 File     : tf-a-stm32mp157f-dk2-usb.stm32

 Size     : 225572 Bytes

 Partition ID : 0x01

​

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

​

File download complete

Time elapsed during download operation: 00:00:00.479

​

RUNNING Program ...

 PartID:   :0x01

Start operation done successfully at partition 0x01

​

Flashlayout Programming ...

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

Running Flashlayout Partition ...

Flashlayout partition started successfully

​

​

Memory Programming ...

Opening and parsing file: fip-stm32mp157f-dk2-trusted.bin

 File     : fip-stm32mp157f-dk2-trusted.bin

 Size     : 1067362 Bytes

 Partition ID : 0x03

​

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

​

File download complete

Time elapsed during download operation: 00:00:01.548

​

RUNNING Program ...

 PartID:   :0x03

​

Reconnecting the device ...

​

USB speed  : High Speed (480MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,

SN     : 002700363030510D32313933

FW version : 0x0110

Device ID  : 0x0500

Start operation done successfully at partition 0x03

​

​

Memory Programming ...

Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32

 File     : tf-a-stm32mp157f-dk2-sdcard.stm32

 Size     : 225445 Bytes

 Partition ID : 0x04

​

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

​

File download complete

Time elapsed during download operation: 00:00:00.062

​

RUNNING Program ...

 PartID:   :0x04

Start operation done successfully at partition 0x04

​

​

Memory Programming ...

Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32

 File     : tf-a-stm32mp157f-dk2-sdcard.stm32

 Size     : 225445 Bytes

 Partition ID : 0x05

​

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

​

File download complete

Time elapsed during download operation: 00:00:00.066

​

RUNNING Program ...

 PartID:   :0x05

Start operation done successfully at partition 0x05

​

​

Memory Programming ...

Opening and parsing file: fip-stm32mp157f-dk2-trusted.bin

 File     : fip-stm32mp157f-dk2-trusted.bin

 Size     : 1067362 Bytes

 Partition ID : 0x06

​

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロアアア 94%

​

Error: failed to download Segment[0]

Error: failed to download the File

Error: Download partition 0x06 failed

Error: TSV flashing service failed

​

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
July 12, 2021

Hi,

did you try using another computer, another board supply, another USB cable ?

Otherwise, could you try if using the attached Flashlayout file file would help ?

FlashLayout_sdcard_stm32mp157f-dk2-trusted(trial).tsv file should be extracted from attached .zip and copied in flashlayout_st-image-weston/trusted/ folder, and then use the following command:

STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157f-dk2-trusted(trial).tsv

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

5 replies

PatrickF
PatrickFBest answer
ST Employee
July 12, 2021

Hi,

did you try using another computer, another board supply, another USB cable ?

Otherwise, could you try if using the attached Flashlayout file file would help ?

FlashLayout_sdcard_stm32mp157f-dk2-trusted(trial).tsv file should be extracted from attached .zip and copied in flashlayout_st-image-weston/trusted/ folder, and then use the following command:

STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157f-dk2-trusted(trial).tsv

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
rbarris
Associate II
March 4, 2023

@PatrickF​ Hi Patrick, I just experienced the same type of problem using the same board: STM32MP157F-DK2.

Have its USB-C power connected to a dedicated USB-C brick (Apple laptop charger). USB-C OTG port plugged into Linux host PC by single cable to a USB3 port.

Errors looked like this - would get partway through this partition each time, failing at a random percentage..

RUNNING Program ... 
 PartID: :0x08 
Start operation done successfully at partition 0x08
 
 
Memory Programming ...
Opening and parsing file: st-image-bootfs-openstlinux-weston-stm32mp1.ext4
 File : st-image-bootfs-openstlinux-weston-stm32mp1.ext4
 Size : 64.00 MB 
 Partition ID : 0x10 
 
Download in Progress:
[====== ] 12% 
 
Error: failed to download Segment[0]
Error: failed to download the File
Error: Download partition 0x10 failed
Error: TSV flashing service failed

I grabbed your trial TSV and was able to flash successfully through DFU. IMO that rules out cables, power, host PC etc etc. (well it completed flashing, but it cannot actually boot... see below)

But this is March 2023 and I'm using the 4.1.0 starter package from ST website.. so I have some doubts as to whether using the hacked TSV from a couple years ago is best practice.. instead can we articulate what modifications if any, should be applied to the flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157f-dk2-trusted.tsv which is included in today's Starter Package ?

en.FLASH-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/images
DL from here
https://www.st.com/en/embedded-software/stm32mp1starter.html
 
starter package process here
https://wiki.st.com/stm32mpu/wiki/STM32MP15_Discovery_kits_-_Starter_Package
 
device listing:
~/stmp2/en.FLASH-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23/images$ STM32_Programmer_CLI -l usb
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.13.0
 -------------------------------------------------------------------
 
===== DFU Interface =====
 
Total number of available STM32 device in DFU mode: 1
 
 Device Index : USB1
 USB Bus Number : 001
 USB Address Number : 003
 Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
 Serial number : 003200193438511836383238
 Firmware version : 0x0110
 Device ID : 0x0500

today's TSV from en.FLASH-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23

more flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157f-dk2-trusted.tsv 
#Opt	Id	Name	Type	IP	Offset	Binary
-	0x01	fsbl-boot	Binary	none	0x0	arm-trusted-firmware/tf-a-stm32mp157f-dk2-usb.stm32
-	0x03	fip-boot	FIP	none	0x0	fip/fip-stm32mp157f-dk2-trusted.bin
P	0x04	fsbl1	Binary	mmc0	0x00004400	arm-trusted-firmware/tf-a-stm32mp157f-dk2-sdcard.stm32
P	0x05	fsbl2	Binary	mmc0	0x00044400	arm-trusted-firmware/tf-a-stm32mp157f-dk2-sdcard.stm32
P	0x06	metadata1	Binary	mmc0	0x00084400	arm-trusted-firmware/metadata.bin
P	0x07	metadata2	Binary	mmc0	0x000C4400	arm-trusted-firmware/metadata.bin
P	0x08	fip-a	FIP	mmc0	0x00104400	fip/fip-stm32mp157f-dk2-trusted.bin
PED	0x09	fip-b	FIP	mmc0	0x00504400	none
PED	0x0A	u-boot-env	Binary	mmc0	0x00904400	none
P	0x10	bootfs	System	mmc0	0x00984400	st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P	0x11	vendorfs	FileSystem	mmc0	0x04984400	st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P	0x12	rootfs	FileSystem	mmc0	0x05984400	st-image-weston-openstlinux-weston-stm32mp1.ext4
P	0x13	userfs	FileSystem	mmc0	0x105984400	st-image-userfs-openstlinux-weston-stm32mp1.ext4

 Results of trying to boot using a DFU-flashed card using the "trial" TSV.. it's unhappy about missing partitions. Which leads me back to wanting to figure out what modification is needed to the modern TSV that came in the starter package..

NOTICE: CPU: STM32MP157FAC Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157F-DK2 Discovery Board
NOTICE: Board: MB1272 Var4.0 Rev.C-02
INFO: PMIC version = 0x20
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.6-stm32mp1-r2.0(debug):v2.6-dirty(a1f02f4f)
NOTICE: BL2: Built : 13:14:26, Nov 23 2021
ERROR: Unable to find a metadata partition
WARNING: Failed to set reference to image id=12 (-2)
WARNING: loading of FWU-Metadata failed, using Bkup-FWU-Metadata
ERROR: Unable to find a metadata partition
WARNING: Failed to set reference to image id=13 (-2)
ERROR: loading of Bkup-FWU-Metadata failed

rbarris
Associate II
March 4, 2023

I eventually did succeed in DFU flashing with the unmodified TSV file from the current day starter package for 4.1.0 (and it does boot properly). But it was very flaky, took half a dozen tries. I hope I don't have to do that very often.

KNono
KNonoAuthor
Associate II
July 13, 2021

Dear PatrickF,

Thank you for your quick response.

It was success with your new file.

Start operation done successfully at partition 0x13

Flashing service completed successfully

I can move to next step.

Thank you!

[full log]

C:\Users\nonoguchi\clickplus_nodered\Starter-Package\stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31\images\stm32mp1>STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157f-dk2-trusted(trial).tsv

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.7.0

   -------------------------------------------------------------------

USB speed  : High Speed (480MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000

SN     : 002700363030510D32313933

FW version : 0x0110

Device ID  : 0x0500

Device name : STM32MP1

Device type : MPU

Device CPU : Cortex-A7

Start Embedded Flashing service

Memory Programming ...

Opening and parsing file: tf-a-stm32mp157c-dk2-usb.stm32

 File     : tf-a-stm32mp157c-dk2-usb.stm32

 Size     : 225572 Bytes

 Partition ID : 0x01

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

File download complete

Time elapsed during download operation: 00:00:00.464

RUNNING Program ...

 PartID:   :0x01

Start operation done successfully at partition 0x01

Flashlayout Programming ...

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

Running Flashlayout Partition ...

Flashlayout partition started successfully

Memory Programming ...

Opening and parsing file: fip-stm32mp157c-dk2-trusted.bin

 File     : fip-stm32mp157c-dk2-trusted.bin

 Size     : 1066932 Bytes

 Partition ID : 0x03

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

File download complete

Time elapsed during download operation: 00:00:01.445

RUNNING Program ...

 PartID:   :0x03

Reconnecting the device ...

USB speed  : High Speed (480MBit/s)

Manuf. ID  : STMicroelectronics

Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,

SN     : 002700363030510D32313933

FW version : 0x0110

Device ID  : 0x0500

Start operation done successfully at partition 0x03

Memory Programming ...

Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32

 File     : tf-a-stm32mp157f-dk2-sdcard.stm32

 Size     : 225445 Bytes

 Partition ID : 0x04

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

File download complete

Time elapsed during download operation: 00:00:00.076

RUNNING Program ...

 PartID:   :0x04

Start operation done successfully at partition 0x04

Memory Programming ...

Opening and parsing file: tf-a-stm32mp157f-dk2-sdcard.stm32

 File     : tf-a-stm32mp157f-dk2-sdcard.stm32

 Size     : 225445 Bytes

 Partition ID : 0x05

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

File download complete

Time elapsed during download operation: 00:00:00.078

RUNNING Program ...

 PartID:   :0x05

Start operation done successfully at partition 0x05

Memory Programming ...

Opening and parsing file: fip-stm32mp157f-dk2-trusted.bin

 File     : fip-stm32mp157f-dk2-trusted.bin

 Size     : 1067362 Bytes

 Partition ID : 0x06

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

File download complete

Time elapsed during download operation: 00:00:00.454

RUNNING Program ...

 PartID:   :0x06

Start operation done successfully at partition 0x06

Memory Programming ...

Opening and parsing file: st-image-bootfs-openstlinux-weston-stm32mp1.ext4

 File     : st-image-bootfs-openstlinux-weston-stm32mp1.ext4

 Size     : 64 MBytes

 Partition ID : 0x10

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

File download complete

Time elapsed during download operation: 00:00:25.330

RUNNING Program ...

 PartID:   :0x10

Start operation done successfully at partition 0x10

Memory Programming ...

Opening and parsing file: st-image-vendorfs-openstlinux-weston-stm32mp1.ext4

 File     : st-image-vendorfs-openstlinux-weston-stm32mp1.ext4

 Size     : 16 MBytes

 Partition ID : 0x11

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

File download complete

Time elapsed during download operation: 00:00:07.381

RUNNING Program ...

 PartID:   :0x11

Start operation done successfully at partition 0x11

Memory Programming ...

Opening and parsing file: st-image-weston-openstlinux-weston-stm32mp1.ext4

 File     : st-image-weston-openstlinux-weston-stm32mp1.ext4

 Size     : 558320 KBytes

 Partition ID : 0x12

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

File download complete

Time elapsed during download operation: 00:04:23.865

RUNNING Program ...

 PartID:   :0x12

Start operation done successfully at partition 0x12

Memory Programming ...

Opening and parsing file: st-image-userfs-openstlinux-weston-stm32mp1.ext4

 File     : st-image-userfs-openstlinux-weston-stm32mp1.ext4

 Size     : 128 MBytes

 Partition ID : 0x13

Download in Progress:

ロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロロ 100%

File download complete

Time elapsed during download operation: 00:01:00.156

RUNNING Program ...

 PartID:   :0x13

Start operation done successfully at partition 0x13

Flashing service completed successfully