Skip to main content
YRink.1
Associate II
January 18, 2021
Question

Exit Low Power Mode M4 via CAN

Hi,

i have a question regarding to exit the Low Power Mode on CM4. Is it possible that i can exit the CStop or CStandby Mode via an Rx Messages of the CAN Bus, when the CAN Bus is assigned to the M4. Iam confused because almost every Bus is listed in https://wiki.st.com/stm32mpu/wiki/Coprocessor_power_management as Wake Up Source except the CAN Bus.

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
January 18, 2021

I confirm, the HW does not permit that.

See STM32MP15x Reference Manual, PWR section.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent