Skip to main content
Associate
Sep 16, 2026 8:15 AM UTC
Question

Evaluation of Display GRAM Functionality

Evaluation of Display GRAM Functionality
The STM32MP157F-DK2 development board is equipped with an OTM8009A display.

Link:

Display panels hardware components - stm32mpu

This IC includes GRAM storage, which theoretically supports maintaining the display output even after the MPU enters sleep mode.

Are there any available test results or evaluation conclusions regarding this?

5 replies

Hank777Author
Associate
Sep 16, 2026 8:21 AM UTC

OTM8009A datasheet:OTM8030A

OTM8009A features a 1244160-byte (480 x 864 x 24 / 8) Graphic RAM (GRAM).

 

A block of RAM integrated within the LCD display controller used to store pixel data for display.

 

Hank777Author
Associate
Sep 18, 2026 12:48 AM UTC

Has anyone tested the GRAM self-refresh function under low-power conditions?

PatrickF
ST Employee
Sep 18, 2026 1:02 PM UTC

Hi ​@Hank777 

 

The STM32MP157F-DK2 hardware and associated starter package has not been optimized for low.
It might be possible to tailor SW settings to keep display available during low-power modes (I guess currently Linux will stop the associated drivers and backlight, so screen became black).

 

Nevertheless, as the display keep the image when you press and maintain the reset button, I’m confident it will be possible to do it in low power with SW adaptations (I’m not SW expert, so I let you dig into https://wiki.st.com/stm32mpu/wiki/How_to_define_your_low-power_strategy.

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Hank777Author
Associate
Sep 20, 2026 6:38 AM UTC

Hi ​@PatrickF 

Thank you for the valuable information; it was very helpful.

Nevertheless, as the display keep the image when you press and maintain the reset button

Hank777Author
Associate
Sep 23, 2026 5:33 AM UTC

Hi ​@PatrickF 

could you help check follow question?

In the STM32MP157F-DK2 environment, the otm8009a driver operates in MIPI-DSI video mode. To utilize the otm8009a's GRAM self-refresh function, it is necessary to switch to command mode. Does the STM32MP157F-DK2 have a command mode driver for the otm8009a?