Skip to main content
AZAMA
Associate
May 21, 2019
Question

Ethernet server with Apache2/PHP/MYSQL/PhpMyAdmin (LAMPP)

Hello,

I'm currently working into STM32MP157C-DK2 and I have made my own image with the following append:

apache2 php phpmyadmin php-cli mysql5

But into my internet page (move from //usr/share/.. to another directory) php code didn't work and when I try to configure mysql5 I have this

ERROR 2002 (HY000): Can't connect to local MySQL server through socket '/var/lib/mysql/mysql.sock' (2)

Also I try to add php-modphp but the bitbake fail

I try too to install dev-pkgs but I get an error too

Do you have any idea ?

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
June 24, 2019

Hi @AZAMA​ 

Sorry for late reply.

Is this post still valid ?

Most of the module you mentioned are by default integrated to the default OpenSTLinux running on DK2 through meta-oe and meta-webserver layers.

Could then please be more specific on what you have done to generate your own image and share the logs in case of errors.

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.