Skip to main content
DmnSd
Associate III
March 22, 2023
Question

Error: Illegal access to ... when flashing custom board with own configuration/device tree

Hello,

I want to upgrade my hardware to new openstlinux kirkstone release november 2022.

First test on eval board was successful.

I have written custom device tree files and compiling for tf-a, u-boot, fip and kernel is fine.

However when I try to flash my image flashlayout to my custom board I get a "ERROR: Illegal access to 0xfffffff0:"

See following for complete output:

NOTICE: CPU: STM32MP157C?? Rev.Z

NOTICE: Model: OSD32MP1 epis shuttle sps board

INFO:   PMIC version = 0x21

INFO:   Reset reason (0x214):

INFO:     IWDG2 Reset (rst_iwdg2)

INFO:   FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000

INFO:   FCONF: Reading firmware configuration information for: stm32mp_io

INFO:   Using USB

INFO:     Instance 2

INFO:   Boot used partition fsbl1

NOTICE: BL2: v2.6-stm32mp1-r2.0(debug):v2.6-dirty(a1f02f4f)

NOTICE: BL2: Built : 13:14:26, Nov 23 2021

INFO:   BL2: Doing platform setup

INFO:   RAM: DDR3-DDR3L 16bits 533000Khz

INFO:   Memory size = 0x20000000 (512 MB)

INFO:   DFU USB START...

INFO:   phase ID :3, Manifestation 3 at c7110ac2

INFO:   Send detach request

INFO:   Receive DFU Detach

INFO:   DFU USB STOP...

INFO:   BL2: Loading image id 1

INFO:   Loading image id=1 at address 0x2ffff000

INFO:   Image id=1 loaded: 0x2ffff000 - 0x2ffff226

INFO:   FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000

INFO:   FCONF: Reading firmware configuration information for: dyn_cfg

INFO:   FCONF: Reading firmware configuration information for: stm32mp1_firewall

INFO:   BL2: Loading image id 4

INFO:   Loading image id=4 at address 0x2ffc5000

INFO:   Image id=4 loaded: 0x2ffc5000 - 0x2ffd9820

INFO:   BL2: Skip loading image id 8

INFO:   BL2: Skip loading image id 9

INFO:   BL2: Loading image id 2

INFO:   Loading image id=2 at address 0xc0500000

INFO:   Image id=2 loaded: 0xc0500000 - 0xc05140a8

INFO:   BL2: Loading image id 16

INFO:   Loading image id=16 at address 0x2ffc0000

INFO:   Image id=16 loaded: 0x2ffc0000 - 0x2ffc39a0

INFO:   BL2: Loading image id 5

INFO:   Loading image id=5 at address 0xc0100000

INFO:   Image id=5 loaded: 0xc0100000 - 0xc01e4534

NOTICE: BL2: Booting BL32

INFO:   Entry point address = 0x2ffc5000

INFO:   SPSR = 0x1d3

NOTICE: SP_MIN: v2.6-stm32mp1-r2.0(debug):v2.6-dirty(a1f02f4f)

NOTICE: SP_MIN: Built : 13:14:26, Nov 23 2021

INFO:   ARM GICv2 driver initialized

INFO:   Set calibration timer to 60 sec

INFO:   stm32mp1 IWDG1 is secure

INFO:   SP_MIN: Initializing runtime services

INFO:   SP_MIN: Preparing exit to normal world

ERROR:  Illegal access to 0xfffffff0:

ERROR:     FAIL_ID = 0x4c0

ERROR:     Non-Secure

ERROR:     Privilege

ERROR:     Read

PANIC at PC : 0x2ffc9739

Exception mode=0x00000016 at: 0x2ffc9739

What is wrong in my configuration or device tree?

Error messages come from tf-a, not sure if it is related to u-boot and fip.

Any suggestion is appreciated! Thanks!

Greez Dmn

This topic has been closed for replies.

1 reply

Olivier GALLIEN
ST Technical Moderator
April 7, 2023

Hi @DmnSd​ 

Sorry to come late in this thread ?

Where do you stand with this issue ?

Did you find the issue ?

I read you are using OSD32MP1. Did you try to contact Octavo support ?

Did you migrate to kirkstone release from ST material or Octavo ones ?

Did your system works properly with previous version ?

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.