Skip to main content
Associate II
September 19, 2023
Question

Encountering Issues with Obtaining ADC Values via DMA

Hi All,

I have an question when i used STM32MP157.

I encountered an issue when using DMA to store the values of ADC conversions.

When I store the data from the ADC_DMA_Buffer to the ADC_DATA_Buffer in the HAL_ADC_ConvCpltCallback() function.

Then check the buffer values using STM32CubeIDE.

I notice that the ADC_DMA_Buffer[1] and ADC_DATA_Buffer[1], ADC_DATA_Buffer[3] ... do not match.

What could be the reason for this?

 

Here is the code and ADC1 configuration: (TIM2 frequency is 1000 Hz (1ms))

 

uint32_t ADC_DMA_Buffer[2] ={0};
uint32_t ADC_DATA_Buffer[500] ={0};
uint16_t ADC_Conversion_Done_Count = 0;

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
 if(hadc->Instance == ADC1)
 {
 ADC_DATA_Buffer[ADC_Conversion_Done_Count] = ADC_DMA_Buffer[0];
 ADC_Conversion_Done_Count++;
 ADC_DATA_Buffer[ADC_Conversion_Done_Count] = ADC_DMA_Buffer[1];
 ADC_Conversion_Done_Count++;
 ADC_Conversion_Done_Count = ADC_Conversion_Done_Count % 500; 
 }
}

int main(void)
{
 HAL_Init();

 if(IS_ENGINEERING_BOOT_MODE())
 {
 SystemClock_Config();
 }
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC1_Init();
 MX_ADC2_Init();
 MX_TIM2_Init();

 /* Run the ADC linear calibration in single-ended mode */
 if (HAL_ADCEx_Calibration_Start(&hadc1,ADC_CALIB_OFFSET_LINEARITY, ADC_SINGLE_ENDED) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_ADCEx_Calibration_Start(&hadc2,ADC_CALIB_OFFSET_LINEARITY, ADC_SINGLE_ENDED) != HAL_OK)
 {
 Error_Handler();
 }

 /* Start ADC conversion */
 if (HAL_ADC_Start(&hadc2) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_ADCEx_MultiModeStart_DMA(&hadc1, ADC_DMA_Buffer, 2) != HAL_OK)
 {
 Error_Handler();
 }

 /* Start Timer */
 HAL_TIM_Base_Start(&htim2);

 while (1)
 {
 }
}

 

 

 

static void MX_ADC1_Init(void)
{
 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};

 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 2;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T2_TRGO;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure the ADC multi-mode
 */
 multimode.Mode = ADC_DUALMODE_INTERL;
 multimode.DualModeData = ADC_DUALMODEDATAFORMAT_DISABLED;
 multimode.TwoSamplingDelay = ADC_TWOSAMPLINGDELAY_5CYCLES;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel */
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
}

 

 

 Best Regards,

Ken

This topic has been closed for replies.