Skip to main content
Mahendra Sondagar
Associate III
February 2, 2021
Question

Enabling the PPP on STM32MP1DK2 board

Hi.... there

Hope you all are doing well

From past few days, I'm playing with STM32MP1

I need to integrate the Quectel EG25G module with the image having ppp functionality

To do so, i have enable ppp support at Make-menuconfig and build the image

Now the problem is, after building the image from scratch, i haven't found the directory /etc/ppp

Even i have also try with the installation from apt-get

But unfortunately, it's not working

Any suggestions ?

Thanks

This topic has been closed for replies.

2 replies

allard
Senior
February 2, 2021

Are you using a correct recipe?

MWoło.2
Senior III
May 10, 2022

Do you have any progress?