Skip to main content
DBuer
Associate II
August 29, 2019
Solved

Enable SPI4 on Linux Side of STM32MP157C-DK2

I would like to access a SPI Device (Ethercat Shield) over the Arduino Headers (SPI4). What do i have to do to get the /dev/spidev... device file in Linux ?

Sorry, but i'm still confused what is enabled, what do i have to enable in DTS files and when i have to rebuild the kernel (that works :) )

Thanks Daniel

This topic has been closed for replies.
AntonioST
AntonioSTBest answer
ST Employee
August 30, 2019

You can use this DT fragment to enable spidev on spi4

&spi4 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&spi4_pins_a>;
	pinctrl-1 = <&spi4_sleep_pins_a>;
	status = "okay";
	cs-gpios = <&gpioe 11 0>;
 
	spidev@0{
		compatible = "spidev";
		reg = <0>;
		spi-max-frequency = <4000000>;
		#address-cells = <1>;
		#size-cells = <0>;
	};
};

4 replies

AntonioST
AntonioSTBest answer
ST Employee
August 30, 2019

You can use this DT fragment to enable spidev on spi4

&spi4 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&spi4_pins_a>;
	pinctrl-1 = <&spi4_sleep_pins_a>;
	status = "okay";
	cs-gpios = <&gpioe 11 0>;
 
	spidev@0{
		compatible = "spidev";
		reg = <0>;
		spi-max-frequency = <4000000>;
		#address-cells = <1>;
		#size-cells = <0>;
	};
};

Visitor II
September 29, 2024

Hi Antonio,

 

I am currently reviewing one of the Linux kernel files (included in the latest Linux 6.1 source provided with OpenSTLinux SDK), called stm32mp1-op~stm32mp-r2-r0/linux-6.1.82/arch/arm/boot/dts/stm32mp15-pinctrl.dtsi.

It seems that the definitions are outdated. There is definitely no "spi4_sleep_pins_a," so the example shown here several times causes the Linux kernel compilation error.

Since I confirmed that my board, through UBOOT, boots files dependent on stm32mp157c-dk2, I added a section with SPI4 at the end of stm32mp157c-dk2.dtb to run an example from the page "How to use SPI from Linux userland with spidev". Unfortunately, during kernel compilation, I get the following error:

 

arch/arm/boot/dts/stm32mp151.dtsi:1397.23-1410.6: ERROR (phandle_references): /soc/etzpc@5c007000/spi@44005000: Reference to non-existent node or label "spi4_sleep_pins_a"

 

 

I am not sure if the statement "On the STM32MP157X-DKX discovery board, MOSI and MISO signals are accessible via the D12 and D11 pins" is still valid with respect to the definitions contained in the DTSI file.

 

Could you provide corrections or guidance on how to run the SPI loopback example using the latest version of OpenSTLinux and the Linux kernel 6.1.88?

 

DBuer
DBuerAuthor
Associate II
August 30, 2019

Thanks a lot