Skip to main content
This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
January 31, 2022

Hi,

USB high-speed (OTG on USB_DM2/DP2 pins) should be used to load either complete image or only up to u-Boot (to use Ethernet as proposed by @Community member​ ).

CubeProgrammer could be used. As not the fastest tool for a complete image, could be used for TF-A/u-Boot load before Ethernet use (I think from u-Boot, an USB Flash drive connected on USBH on USB_DM1/DP1 might be possible).

All these might need some small tailoring or scripting of our standard deliveries.

Alternatively, especially if you don't want to use Ethernet, our partner Elprotronic also provide a fast USB flasher: https://www.elprotronic.com/pages/gangflasher-st

For eMMC pin choices, i confirm the only restrictions are the 3 pins used by BootROM (and obviously the AFmux possibilities regarding other eMMC pins). See also AN5031 for more guidelines.

Regards,

Patrick

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

7 replies

Tesla DeLorean
Guru
January 30, 2022

Other Embedded Linux platforms had minimal u-Boot use Ethernet to pull, or stream data loop, from a server

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PatrickF
PatrickFBest answer
ST Employee
January 31, 2022

Hi,

USB high-speed (OTG on USB_DM2/DP2 pins) should be used to load either complete image or only up to u-Boot (to use Ethernet as proposed by @Community member​ ).

CubeProgrammer could be used. As not the fastest tool for a complete image, could be used for TF-A/u-Boot load before Ethernet use (I think from u-Boot, an USB Flash drive connected on USBH on USB_DM1/DP1 might be possible).

All these might need some small tailoring or scripting of our standard deliveries.

Alternatively, especially if you don't want to use Ethernet, our partner Elprotronic also provide a fast USB flasher: https://www.elprotronic.com/pages/gangflasher-st

For eMMC pin choices, i confirm the only restrictions are the 3 pins used by BootROM (and obviously the AFmux possibilities regarding other eMMC pins). See also AN5031 for more guidelines.

Regards,

Patrick

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
cfilipescu
Senior
March 1, 2022

@PatrickF​ 

Is it not possible to flash the nand or emmc from a linux boot on the sdcard? That way this would not require any external devices and just an SDcard?

JDave.4
JDave.4Author
Associate III
January 31, 2022

Hi all,

Thanks for the replies. Is it possible to use ST Link v3 to program a blank eMMC? If so, what could be max. transfer rate?

PatrickF
ST Employee
January 31, 2022

Hi,

unlike STM32 MCUs, it is not possible to flash STM32MP1 products using ST-Link.

On STM32 MPUs, ST-Link is only used for debug purposes (e.g. with CubeIDE).

Only UART or USB (OTG on USB_DP2/DM2) are supported for flashing.

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent