Skip to main content
asadullah4571
Associate III
August 8, 2024
Solved

EMMC device 0 not found

i try to flash starter package to our mmc but the error is found i done step by step

in botton text i bold the error please check it once and help me out why this is happend. 

 

 

 

 

10:55:11 : UR connection mode is defined with the HWrst reset mode
10:55:11 : USB speed : High Speed (480MBit/s)
10:55:11 : Manuf. ID : STMicroelectronics
10:55:11 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
10:55:11 : SN : 004200273132511831373339
10:55:11 : DFU protocol: 1.1
10:55:11 : Board : --
10:55:11 : Device ID : 0x0500
10:55:11 : Start Embedded Flashing service
10:55:11 : Memory Programming ...
10:55:11 : Opening and parsing file: tf-a-stm32mp157f-dk2-usb.stm32
10:55:11 : File : tf-a-stm32mp157f-dk2-usb.stm32
10:55:11 : Size : 220.41 KB
10:55:11 : Partition ID : 0x01
10:55:11 : Download in Progress:
10:55:13 : File download complete
10:55:13 : Time elapsed during download operation: 00:00:01.818
10:55:13 : RUNNING Program ...
10:55:13 : PartID: :0x01
10:55:13 : Start operation done successfully at partition 0x01
10:55:13 : Memory Programming ...
10:55:13 : Opening and parsing file: fip-stm32mp157f-dk2-optee-sdcard.bin
10:55:13 : File : fip-stm32mp157f-dk2-optee-sdcard.bin
10:55:13 : Size : 1.40 MB
10:55:13 : Partition ID : 0x03
10:55:13 : Download in Progress:
10:55:15 : File download complete
10:55:15 : Time elapsed during download operation: 00:00:01.548
10:55:15 : RUNNING Program ...
10:55:15 : PartID: :0x03
10:55:15 : Reconnecting the device ...
10:55:19 : USB speed : High Speed (480MBit/s)
10:55:19 : Manuf. ID : STMicroelectronics
10:55:19 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
10:55:19 : SN : 004200273132511831373339
10:55:19 : DFU protocol: 1.1
10:55:19 : Board : --
10:55:19 : Device ID : 0x0500
10:55:19 : Device name : STM32MP157FAC Rev.Z
10:55:19 : Device type :
10:55:19 : Device CPU :
10:55:19 : Start operation done successfully at partition 0x03
10:55:19 : Flashlayout Programming ...
10:55:19 : Running Flashlayout Partition ...
10:55:19 : Reconnecting the device ...
10:55:19 : USB speed : High Speed (480MBit/s)
10:55:19 : Manuf. ID : STMicroelectronics
10:55:19 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
10:55:19 : SN : 004200273132511831373339
10:55:19 : DFU protocol: 1.1
10:55:19 : Board : --
10:55:19 : Device ID : 0x0500
10:55:19 : Device name : STM32MP157FAC Rev.Z
10:55:19 : Device type :
10:55:19 : Device CPU :
10:55:19 : Flashlayout partition started successfully
10:55:19 : Error: Message from Embedded Flash Loader : mmc device 0 not found
10:55:19 : Received PhaseID == 0xFF, system is going to reboot
10:55:19 : Start Embedded Flashing service
10:55:19 : Error: Message from Embedded Flash Loader : mmc device 0 not found
10:55:19 : Received PhaseID == 0xFF, system is going to reboot

This topic has been closed for replies.
Gregory PLANCHON
Gregory PLANCHONBest answer
ST Technical Moderator
August 8, 2024

hi @asadullah4571,

 

There is no eMMC on boards stm32mp157f-dk2.

 

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Gregory PLANCHON
Gregory PLANCHONBest answer
ST Technical Moderator
August 8, 2024

hi @asadullah4571,

 

There is no eMMC on boards stm32mp157f-dk2.

 

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.