DSI display comes up during U-Boot and displays ST Logo but turns off once Linux Kernel takes over on our custom DK2 board. Weston Wayland Compositor fails to start during boot and backlight setup fails too. Does Wayland compositor have GPIO dependen
- 3 replies
- 2308 views
Most of the DSI pin mapping is same as ST's DK2 board except DSI_RESET and DSI_TE. I updated the DSI_RESET pin mapping in the device tree to reflect actual connections. However, Weston Wayland compositor fails to start even when DSI display is not connected. Does weston have any other GPIO dependencies?
[ 2.289892] stm32-usbphyc 5a006000.usbphyc: registered rev:1.0
[ 2.295603] stm32-display-dsi 5a000000.dsi: Linked as a consumer to regulator.2
[ 2.304123] panel-orisetech-otm8009a 5a000000.dsi.0: Linked as a consumer to regulator.8
[FAILED] Failed to start Weston Wayland Compositor.
[FAILED] Failed to start Load/Save Screen Ba…tness of backlight:5a000000.dsi.0.
I get the following messages when I try to manually start weston:
root@stm32mp1:/sbin# weston start
Date: 2020-01-29 UTC
[21:20:37.923] weston 5.0.0
https://wayland.freedesktop.org
Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
Build: unknown (not built from git or tarball)
[21:20:37.923] Command line: weston start
[21:20:37.923] OS: Linux, 4.19.49, #1 SMP PREEMPT Sun Jun 9 07:17:25 UTC 2019, armv7l
[21:20:37.924] Using config file '/etc/xdg/weston/weston.ini'
[21:20:37.925] Output repaint window is 100 ms maximum.
[21:20:37.925] Loading module '/usr/lib/libweston-5/drm-backend.so'
[21:20:37.940] initializing drm backend
[21:20:37.941] logind: failed to get session seat
[21:20:37.942] logind: cannot setup systemd-logind helper (-61), using legacy fallback
[21:20:37.942] <stdin> not a vt
[21:20:37.942] if running weston from ssh, use --tty to specify a tty
[21:20:37.942] fatal: drm backend should be run using weston-launch binary, or your system should provide the logind D-Bus API.
[21:20:37.942] fatal: failed to create compositor backend
The output of 'systemctl status weston.service'
[[0;1;31m�?[[0m weston.service - Weston Wayland Compositor
Loaded: loaded (/lib/systemd/system/weston.service; enabled; vendor preset: enabled)
Active: [[0;1;31mfailed[[0m (Result: exit-code) since Wed 2020-01-29 20:59:31 UTC; 22min ago
Process: 3609 ExecStartPre=/sbin/check-gpu [[0;1;31m(code=exited, status=1/FAILURE)[[0m
Jan 29 20:59:31 stm32mp1 systemd[1]: Starting Weston Wayland Compositor...
Jan 29 20:59:31 stm32mp1 systemd[1]: [[0;1;39m[[0;1;31m[[0;1;39mweston.service: Control process exited, code=exited status=1[[0m
Jan 29 20:59:31 stm32mp1 systemd[1]: [[0;1;39m[[0;1;31m[[0;1;39mweston.service: Failed with result 'exit-code'.[[0m
Jan 29 20:59:31 stm32mp1 systemd[1]: [[0;1;31m[[0;1;39m[[0;1;31mFailed to start Weston Wayland Compositor.[[0m
I've attached full boot log for your reference.