Skip to main content
jhi
Senior
January 17, 2023
Question

DRM/KMS framebuffer emulation - How to set format

Using the KMS/DRM driver, how can I change the emulated framebuffer format? I'm using simple-panel and the framebuffer has always only 16-bit color even though the driver explicit sets the format for 24-bit colors (.bus_format = MEDIA_BUS_FMT_RGB888_1X24).

fbset doesn't work:

fbset -g 800 480 800 480 24
fbset: FBIOPUT_VSCREENINFO: Invalid argument

modetest

modetest -M stm
Encoders:
id crtc type possible crtcs possible clones
32 38 DPI 0x00000001 0x00000001
 
Connectors:
id encoder status name size (mm) modes encoders
33 32 connected DPI-1 154x86 1 32
 modes:
 index name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot
 #0 800x480 57.29 800 1010 1011 1057 480 503 523 545 33000 flags: ; type: preferred, driver
 props:
 1 EDID:
 flags: immutable blob
 blobs:
 
 value:
 2 DPMS:
 flags: enum
 enums: On=0 Standby=1 Suspend=2 Off=3
 value: 0
 5 link-status:
 flags: enum
 enums: Good=0 Bad=1
 value: 0
 6 non-desktop:
 flags: immutable range
 values: 0 1
 value: 0
 4 TILE:
 flags: immutable blob
 blobs:
 
 value:
 
CRTCs:
id fb pos size
38 43 (0,0) (800x480)
 #0 800x480 57.29 800 1010 1011 1057 480 503 523 545 33000 flags: ; type: preferred, driver
 props:
 24 VRR_ENABLED:
 flags: range
 values: 0 1
 value: 0
 31 BACKGROUND_COLOR:
 flags: range
 values: 0 18446744073709551615
 value: 18446462598732840960
 28 GAMMA_LUT:
 flags: blob
 blobs:
 
 value:
 29 GAMMA_LUT_SIZE:
 flags: immutable range
 values: 0 4294967295
 value: 256
 
Planes:
id crtc fb CRTC x,y x,y gamma size possible crtcs
34 38 43 0,0 0,0 0 0x00000001
 formats: AR24 XR24 RG24 RG16 AR15 XR15 AR12 XR12 C8
 props:
 8 type:
 flags: immutable enum
 enums: Overlay=0 Primary=1 Cursor=2
 value: 1
 30 IN_FORMATS:
 flags: immutable blob
 blobs:
 
 value:
 01000000000000000900000018000000
 01000000400000004152323458523234
 52473234524731364152313558523135
 41523132585231324338202000000000
 ff010000000000000000000000000000
 0000000000000000
 in_formats blob decoded:
 AR24: LINEAR
 XR24: LINEAR
 RG24: LINEAR
 RG16: LINEAR
 AR15: LINEAR
 XR15: LINEAR
 AR12: LINEAR
 XR12: LINEAR
 C8 : LINEAR
 36 alpha:
 flags: range
 values: 0 65535
 value: 65535
 37 zpos:
 flags: immutable range
 values: 0 0
 value: 0
39 0 0 0,0 0,0 0 0x00000001
 formats: AR24 RG24 RG16 AR15 AR12 C8
 props:
 8 type:
 flags: immutable enum
 enums: Overlay=0 Primary=1 Cursor=2
 value: 0
 30 IN_FORMATS:
 flags: immutable blob
 blobs:
 
 value:
 01000000000000000600000018000000
 01000000300000004152323452473234
 52473136415231354152313243382020
 3f000000000000000000000000000000
 0000000000000000
 in_formats blob decoded:
 AR24: LINEAR
 RG24: LINEAR
 RG16: LINEAR
 AR15: LINEAR
 AR12: LINEAR
 C8 : LINEAR
 41 alpha:
 flags: range
 values: 0 65535
 value: 65535
 42 zpos:
 flags: immutable range
 values: 1 1
 value: 1
 
Frame buffers:
id size pitch

modetest -M stm -s 33@32:800x480-57.29@XR24 &
# failed to find CRTC for pipe
failed to create dumb buffer: Invalid argument

This topic has been closed for replies.

3 replies

jhi
jhiAuthor
Senior
January 17, 2023

fbset

mode "800x480-0"
 # D: 0.000 MHz, H: 0.000 kHz, V: 0.000 Hz
 geometry 800 480 800 480 16
 timings 0 0 0 0 0 0 0
 accel true
 rgba 5/11,6/5,5/0,0/0
endmode

I also tried to change the kernel driver (drivers/gpu/drm/stm/drv.c), by adding

ddev->mode_config.preferred_depth = 24;

but it didn't change anything.

OlivierK
ST Technical Moderator
January 17, 2023

Hi jhi (Community Member)

According to your settings CRTC ID seems to be equal to 38 (not 32).

What about if you try modetest -M stm -s 33@38:800x480-57.29@XR24 &

Regards,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
jhi
jhiAuthor
Senior
January 18, 2023

Well the command "works" and it shows the test image, but I can't say if it is 24-bit or not because it seems that the mode lasts only as long the modetest is running. If it really sets it persistent, I can't see any difference with my test image and fbset shows the same as before.

# modetest -M stm -s 33@38:800x480-57.29@XR24 -d &
# setting mode 800x480-57.29Hz on connectors 33, crtc 38
 
[1]+ Done modetest -M stm -s 33@38:800x480-57.29@XR24 -d

How can I set this mode to be persistent or default? Are there any other ways to set the framebuffer color depth? Where does the stm kernel driver get the format information? I can see from the driver that it checks which color format is used so how can I change this format?