Skip to main content
坤祁.2387
Associate
December 10, 2019
Question

Does nandflash and EMMC of stm32mp157c share the same interface or independent interface?

..

This topic has been closed for replies.

2 replies

PatrickF
ST Employee
December 10, 2019

Hello,

You could find detail information in Documentations (Reference Manual, DataSheet), Application Note (AN5031) or Wiki (e.g. https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_overview)

To sum-up, we are able to connect simultaneously many interface, if package pin count and your pinout usage allow it (your could quickly test using STM32CubeMx).

e.g. a typical usage similar to STM32MP157C-EV1 board

  • SD-Card 4-bits on SDMMC1
  • eMMC 8-bits on SDMMC2
  • Serial-NOR 4-bits and/or Serial-NAND 4-bits on QUADSPI
  • SLC-NAND 8 or 16-bits on FMC

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
坤祁.2387
Associate
December 18, 2019
The touch screen part of stm32mp157c-dk2 does not need to be interrupted and reset?