Skip to main content
ChipHead
Associate III
June 10, 2020
Solved

Does DK2 include NPU (galcore.ko)?

Recently, I bought STM32MP1 DK2 board. Does DK2 board include NPU (Neural Processing Unit)? Can we use ​the NPU device via galcore.ko (Linux kernel module) to run deep learning network models on the DK2 board? Welcome to any hints and comments.

​

​

BRs,

Geunsik​

​

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
June 12, 2020

Hi @ChipHead​ 

Yes your're right, galcore.ko is the driver for the Vivante GCNANO GPU inside STM32MP157 but does not include NPU.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

5 replies

Olivier GALLIEN
ST Technical Moderator
June 11, 2020

Hi @ChipHead​ 

No STM32MP15 does not include NPU.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
ChipHead
ChipHeadAuthor
Associate III
June 11, 2020

Dear Olivier,​

​

Thank you for your reply. I thought that STM32MP157C (DK2) include a Amlogic/Viavntea NPU because I could see a galcore.ko file on the DK2 board as follows. Is it incorrect? If the board does not include the NPU, what is a goal of the galcore.ko file on DK2 board?

​

​

For example, ​

root@stm32mp1:~# modinfo galcore

filename: /lib/modules/4.19.94/extra/galcore.ko

license: Dual MIT/GPL

description: Vivante Graphics Driver

alias: of:N*T*Cvivante,gcC*

alias: of:N*T*Cvivante,gc

alias: of:N*T*Cst,gcnanoC*

alias: of:N*T*Cst,gcnano

​ ... omission....

​

BRs,

Geunsik Lim

​

​

ChipHead
ChipHeadAuthor
Associate III
June 11, 2020

And, I attached a figure file that describes different features among board models of STM32MP1. As we can see, DK2 (STM32MP1) board includes 3D GPU feature compared to others. I thought that the feature is related to the galcore.ko file.

​

​

BRs,

​

​

​