Skip to main content
TStru.1
Associate II
August 2, 2021
Question

Device Tree configuration for RMII with Crystal on PHY, no 50Mhz from PHY

I am attempting to configure my device tree to support RMII with Crystal on PHY, no 50Mhz from PHY. I have made the following modifications based on https://wiki.st.com/stm32mpu/wiki/Ethernet_device_tree_configuration#RGMII_with_Crystal_on_PHY-2C_no_125Mhz_from_PHY with a 50MHz clock instead of 125Mhz.

Board Specific Linux DTS

&ethernet0 {
	status = "okay";
	pinctrl-0 = <&eth1_pins_mx>;
	pinctrl-1 = <&eth1_sleep_pins_mx>;
	pinctrl-names = "default", "sleep";
	phy-mode = "rmii";
	max-speed = <100>;
	phy-handle = <&phy0>;
 
	mdio0 {
			#address-cells = <1>;
			#size-cells = <0>;
			compatible = "snps,dwmac-mdio";
 
			phy0: ethernet-phy@0 {
				reg = <0>;	
				reset-gpios = <&gpiog 9 GPIO_ACTIVE_LOW>;
				reset-assert-us = <1000>;
				reset-deassert-us = <200000>;
			};
	};
};

stm32mp151.dtsi

ethernet0: ethernet@5800a000 {
	compatible = "st,stm32mp1-dwmac", "snps,dwmac-4.20a";
	reg = <0x5800a000 0x2000>;
	reg-names = "stmmaceth";
	interrupts-extended = <&intc GIC_SPI 61 IRQ_TYPE_LEVEL_HIGH>,
							<&intc GIC_SPI 62 IRQ_TYPE_LEVEL_HIGH>,
							<&exti 70 1>;
	interrupt-names = "macirq",
						"eth_wake_irq",
						"stm32_pwr_wakeup";
	clock-names = "stmmaceth",
					"eth-ck",
					"mac-clk-tx",
					"mac-clk-rx",
					"ethstp";
	clocks = <&rcc ETHMAC>,
				<&rcc ETHCK_K>, 
				<&rcc ETHTX>,
				<&rcc ETHRX>,
				<&rcc ETHSTP>;
	st,syscon = <&syscfg 0x4>;
	snps,mixed-burst;
	snps,pbl = <2>;
	snps,en-tx-lpi-clockgating;
	st,eth-clk-sel;
	snps,axi-config = <&stmmac_axi_config_0>;
	snps,tso;
	power-domains = <&pd_core>;
	status = "disabled";
};

TF-A dts rcc

&rcc {
	st,csi-cal;
	st,hsi-cal;
	st,cal-sec = <60>;
	st,clksrc = <
		CLK_MPU_PLL1P
		CLK_AXI_PLL2P
		CLK_MCU_PLL3P
		CLK_PLL12_HSE
		CLK_PLL3_HSE
		CLK_PLL4_HSE
		CLK_RTC_LSE
		CLK_MCO1_DISABLED
		CLK_MCO2_DISABLED
	>;
	st,clkdiv = <
		1 		/*MPU*/
		0 		/*AXI*/
		0 		/*MCU*/
		1 		/*APB1*/
		1 		/*APB2*/
		1 		/*APB3*/
		1 		/*APB4*/
		2 		/*APB5*/
		0 		/*RTC*/
		0 		/*MCO1*/
		0 		/*MCO2*/
	>;
	st,pkcs = <
		CLK_CKPER_HSE
		CLK_ETH_PLL4P /*CLK_ETH_DISABLED*/
		CLK_SDMMC12_PLL4P
		CLK_STGEN_HSE
		CLK_USBPHY_HSE
		CLK_SPI2S1_DISABLED
		CLK_SPI2S23_PLL3Q
		CLK_SPI45_DISABLED
		CLK_SPI6_DISABLED
		CLK_I2C46_HSI
		CLK_SDMMC3_DISABLED
		CLK_USBO_USBPHY
		CLK_ADC_CKPER
		CLK_CEC_DISABLED
		CLK_I2C12_HSI
		CLK_I2C35_DISABLED
		CLK_UART1_DISABLED
		CLK_UART24_HSI
		CLK_UART35_DISABLED
		CLK_UART6_DISABLED
		CLK_UART78_DISABLED
		CLK_SPDIF_DISABLED
		CLK_FDCAN_HSE
		CLK_SAI1_DISABLED
		CLK_SAI2_DISABLED
		CLK_SAI3_DISABLED
		CLK_SAI4_DISABLED
		CLK_LPTIM1_DISABLED
		CLK_LPTIM23_DISABLED
		CLK_LPTIM45_DISABLED
	>;
	pll2:st,pll@1 {
		compatible = "st,stm32mp1-pll";
		reg = <1>;
		cfg = < 2 65 1 0 0 PQR(1,1,1) >;
		frac = < 0x1400 >;
	};
	pll3:st,pll@2 {
		compatible = "st,stm32mp1-pll";
		reg = <2>;
		cfg = < 1 33 1 16 36 PQR(1,1,0) >;
		frac = < 0x1a04 >;
	};
	pll4:st,pll@3 {
		compatible = "st,stm32mp1-pll";
		reg = <3>;
		/*cfg = < 3 98 5 7 7 PQR(1,1,0) >;*/
		cfg = < 1 49 11 9 9 PQR(1,1,1) >;
	};
};

I get the following result which I believe indicates a clock configuration error based on section 5.3 of https://wiki.st.com/stm32mpu/wiki/Ethernet_overview

[ 17.067472] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Micrel KSZ8081 or KSZ8091] (irq=POLL)
[ 18.094222] stm32-dwmac 5800a000.ethernet: Failed to reset the dma
[ 18.098953] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[ 18.132868] stm32-dwmac 5800a000.ethernet eth0: stmmac_open: Hw setup failed

Is this configuration possible?

This topic has been closed for replies.

1 reply

OlivierK
ST Technical Moderator
August 3, 2021

Hi TStru.1 (Community Member)

In the same page you can find the DT configuration for a RMII configuration with crystal on Phy (3.3.1)

The Ethernet reference clock must come either from RCC or from the 50MHz from the phy to the MAC.

Rgds,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.