Skip to main content
Associate II
Jan 8, 2026 10:10 PM UTC
Question

Debugging Openamp on STM32MP1-DK2

Hi All

I have a question about the debugging the M4 when we are using OpenAMP

 

Lets say we have a simple example from the docs , and i am creating debug config and i am expecting the code to be flashed and the communication to work (while debugging) but that is not the case.

 

What is happening is the following , when debugging the code hangs on MX_OPENAMP_Init(RPMSG_REMOTE, NULL);  and this is because the M4 is a slave and waits for the A7 to send a signal , but that is never happening because the A7 core is not aware of the debug.

 

Is there a straightforward way to debug ? instead of attaching to a running target , restarting the M4 core etc.

I cannot find anything on the internet

 

Thank you