Skip to main content
MNoor.1
Associate II
March 31, 2020
Solved

Debugging Cortex M4 in engineering mode, is it necessary to edit and build device trees for custom modifications?

Hello,

I'm trying to connect stm32mp157c-dk2 board with another device over FDCAN in engineering mode (MCU single core) using CN2 pin 3 and 5 (stm32 PA12 and PA11 pins respectively). Though I can initialize and request to use FDCAN1 from resource manager utility without any error, FDCAN related interrupts still don't get fired. Do I need to assign RX/TX pins to M4 FDCAN1 in tf-a, u-boot or kernel device trees.

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
April 1, 2020

Hi @MNoor.1​ 

In Engeneering mode A7 is on hold and M4 is able to initialize the assigned IPs as per configured in CubeMX.

Thus, not need to change anything on Linux side. ( have to be done when you will move to Production mode)

I guess you should check your FDCAN and related IT settings in CubeMX.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
April 1, 2020

Hi @MNoor.1​ 

In Engeneering mode A7 is on hold and M4 is able to initialize the assigned IPs as per configured in CubeMX.

Thus, not need to change anything on Linux side. ( have to be done when you will move to Production mode)

I guess you should check your FDCAN and related IT settings in CubeMX.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.