Skip to main content
Associate II
Oct 6, 2025 9:17 AM UTC
Question

Custom Setup for STM32MP257f.

 

Hello,

I’m currently rebuilding the device tree (DTS) for our custom board. I’ve modified the pin configurations according to our schematic. Could you please confirm if updating only the following files is sufficient for our customization?

  • stm32mp257f-ev1.dts

  • stm32mp25-pinctrl.dtsi

My understanding is that these two files should cover the required pin configuration changes for our board, and the rest of the device tree files can remain unchanged.

Also, I would like to avoid the consumer=kernel messages that appear when running the command:

 

 
cat /sys/kernel/debug/pinmux-pins/*/pins

Could you please confirm if my approach is correct, or if there are any additional changes needed elsewhere in the device tree?

Best regards,
Preetham.


Please suggest points that help to my work.

This topic has been closed for replies.

5 replies

Erwan SZYMANSKI
ST Technical Moderator
Oct 6, 2025 10:01 AM UTC

Hello @_Krishna ,
Your overall understanding is partially correct.

Indeed, you have to modify what we call the board device tree (DTS) so that the HW configuration matches with your own board. The pinctrl as you mentioned it is to adapt to your needs too, but you can rewrite the pin configuration in your board DTS file.

However, for your own design, sometimes starting from the Evaluation board DTS is a bit tricky. CubeMX tool is supposed to create you all the device tree you need regarding the configuration you set.

Another important point, because it seems that you are targeting the Linux kernel here, but the DTS have to be changed/adapted in every BSP component (Linux, OP-TEE, U-Boot, TF-A) if you hope to get a bootable board at the end.

DDR configuration is also to adapt depending on your design.

Kind regards,
Erwan.

PS: Some useful links:
- https://wiki.st.com/stm32mpu/wiki/How_to_create_STM32MPU_projects_with_STM32CubeMX
- https://wiki.st.com/stm32mpu/wiki/How_to_create_your_product_from_design_to_manufacturing

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
_KrishnaAuthor
Associate II
Oct 6, 2025 10:48 AM UTC

Hii Erwan,
      Thanks for replying your answer is bit tricky for me to understand since I am a beginner can you please elaborate so that I ca understand as a beginner?







Thanks and regards,
Preetham

Erwan SZYMANSKI
ST Technical Moderator
Oct 6, 2025 3:12 PM UTC

Hi @_Krishna ,
Did you already prototype your product on a ST evaluation/discovery kit ? 

I think the first step would be to follow the ST wiki guidelines to get more familiar with the evaluation kit itself. The entry point is here: https://wiki.st.com/stm32mpu/wiki/Getting_started

I think the idea would be manipulate on ST board before to get into your own design software. Then once you well understand how does the OpenSTLinux ecosystem works, you can try to apply this on your own hardware, indeed by changing device trees, DDR config...

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
_KrishnaAuthor
Associate II
Oct 8, 2025 1:56 PM UTC

Hii @Erwan SZYMANSKI,

  Thanks for replying — that means a lot. I was busy. I checked as per your suggestions, and in TFM and U-Boot, they have similar files in their sources. However, those files are unmodified, so I think changing those device trees plays a key role in avoiding this “consumer = kernel” issue.