Skip to main content
Associate III
Oct 5, 2026 7:00 AM UTC
Solved

creating our own Linux OS with OpenSTLinux vs Ubuntu 24.04

Hello ST team and community,

I am developing a custom STM32MP257-based MPU board and I want to create a customized Linux OS for our own product.

I would like to understand the officially recommended approach and the limitations of using OpenSTLinux/Yocto versus an Ubuntu 24.04 ARM64 root filesystem.

My target hardware is:

  • MPU: STM32MP257F
  • Custom PCB/SOM
  • Cortex-A35 used for Linux
  • Cortex-M33 may be used for real-time firmware
  • Custom DDR/LPDDR4 configuration
  • Custom Ethernet/USB/SD/eMMC/UART peripherals
  • Custom Device Tree generated/configured using STM32CubeMX
  • Development host: Ubuntu 24.04 LTS

I understand that ST's current Distribution Package supports STM32MP25x and allows users to create their own Linux distribution.

 

Thank You,

Vijaya.

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Oct 5, 2026 12:10 PM UTC

Hi ​@vijayajangam, 

Yes ST provide and support OpenSTLinux/Yocto. 

Even if possible ST does not provide not support  Ubuntu 24.04. 

I think some community member share similar project. 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

1 reply

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Oct 5, 2026 12:10 PM UTC

Hi ​@vijayajangam, 

Yes ST provide and support OpenSTLinux/Yocto. 

Even if possible ST does not provide not support  Ubuntu 24.04. 

I think some community member share similar project. 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.