Skip to main content
nlbutts
Associate II
July 1, 2019
Question

Creating a bootable SD card with dd

I've tried to create a bootable CD card image using both the Starter image as well as a Yocto built image. In both cases the device fails to boot.

I've gone into stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/images/stm32mp1 directory and then run:

scripts/create_sdcard_from_flashlayout.sh flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-basic.tsv

This creates a .RAW image and instruction on how to load that onto the SD card. I then run:

sudo dd if=flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw of=/dev/sdb bs=8M conv=fdatasync status=progress

When this is done I insert the SD card into the stm32mp157c-dk2 board and set both boot dip switches to on. I then apply power and nothing happens. There is no output on the terminal.

Is this method supported?

This topic has been closed for replies.

3 replies

Olivier GALLIEN
ST Technical Moderator
July 2, 2019

Hi @nlbutts​ 

Yes this is supported

Please refer to User manual to check you didn't forget any step :

https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
nlbutts
nlbuttsAuthor
Associate II
July 2, 2019

Thanks for the response. I followed that page precisely and my board would not boot. I did get it to boot by using the STM32_Programmer_CLI tool. But I would like to simply image an SD card.

PatrickF
ST Employee
July 3, 2019

Hello, did you use a Linux PC or a VM ?

I just tried using VMware without trouble.

On VM, be sure you write to the right SD-Card and this one is visible (use cat /proc/partitions).

~/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/images/stm32mp1/scripts$ ./create_sdcard_from_flashlayout.sh 
../flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-basic.tsv
Create Raw empty image: ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw of 1536MB
Create partition table:
[CREATED] part 1: fsbl1 [partition size 256.0 KiB]
[CREATED] part 2: fsbl2 [partition size 256.0 KiB]
[CREATED] part 3: ssbl [partition size 2.0 MiB]
[CREATED] part 4: bootfs [partition size 64.0 MiB]
[CREATED] part 5: vendorfs [partition size 16.0 MiB]
[CREATED] part 6: rootfs [partition size 750.4 MiB]
[CREATED] part 7: userfs [partition size 703.0 MiB]
 
Partition table from ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw
Disk ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw: 3145728 sectors, 1.5 GiB
Sector size (logical): 512 bytes
Disk identifier (GUID): 1868411E-3CF7-4736-B071-95E882E39B34
Partition table holds up to 128 entries
Main partition table begins at sector 2 and ends at sector 33
First usable sector is 34, last usable sector is 3145694
Partitions will be aligned on 2-sector boundaries
Total free space is 0 sectors (0 bytes)
 
Number Start (sector) End (sector) Size Code Name
 1 34 545 256.0 KiB 8300 fsbl1
 2 546 1057 256.0 KiB 8300 fsbl2
 3 1058 5153 2.0 MiB 8300 ssbl
 4 5154 136225 64.0 MiB 8300 bootfs
 5 136226 168993 16.0 MiB 8300 vendorfs
 6 168994 1705857 750.4 MiB 8300 rootfs
 7 1705858 3145694 703.0 MiB 8300 userfs
 
Populate raw image with image content:
[ FILLED ] part 1: fsbl1, image: u-boot-spl.stm32-stm32mp157c-dk2-basic 
[ FILLED ] part 2: fsbl2, image: u-boot-spl.stm32-stm32mp157c-dk2-basic 
[ FILLED ] part 3: ssbl, image: u-boot-stm32mp157c-dk2-basic.img 
[ FILLED ] part 4: bootfs, image: st-image-bootfs-openstlinux-weston-stm32mp1.ext4 
[ FILLED ] part 5: vendorfs, image: st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 
[ FILLED ] part 6: rootfs, image: st-image-weston-openstlinux-weston-stm32mp1.ext4 
[ FILLED ] part 7: userfs, image: st-image-userfs-openstlinux-weston-stm32mp1.ext4 
 
###########################################################################
###########################################################################
 
RAW IMAGE generated: ../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw
 
WARNING: before to use the command dd, please umount all the partitions
	associated to SDCARD.
 sudo umount `lsblk --list | grep mmcblk0 | grep part | gawk '{ print $7 }' | tr '\n' ' '`
 
To put this raw image on sdcard:
 sudo dd if=../flashlayout_st-image-weston/../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw of=/dev/mmcblk0 bs=8M conv=fdatasync status=progress
 
(mmcblk0 can be replaced by:
 sdX if it's a device dedicated to receive the raw image 
 (where X can be a, b, c, d, e)
 
###########################################################################
###########################################################################
~/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/images/stm32mp1/scripts$ sudo dd if=../flashlayout_st-image-weston_FlashLayout_sdcard_stm32mp157c-dk2-basic.raw of=/dev/sdb bs=8M conv=fdatasync
192+0 records in
192+0 records out
1610612736 bytes (1.6 GB, 1.5 GiB) copied, 82.6478 s, 19.5 MB/s

then when you boot the DK2 platform using this SD-Card, should see on the console (ST-Link VCP)

U-Boot SPL 2018.11-stm32mp-r2 (Nov 14 2018 - 16:10:06 +0000)
Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
RAM: DDR3-1066/888 bin G 1x4Gb 533MHz v1.41
Trying to boot from MMC1
 
 
U-Boot 2018.11-stm32mp-r2 (Nov 14 2018 - 16:10:06 +0000)
 
CPU: STM32MP157CAC Rev.B
Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
Board: stm32mp1 in basic mode (st,stm32mp157c-dk2)
Board: MB1272 Var2 Rev.C-01
 Watchdog enabled
DRAM: 512 MiB
.......

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent