Skip to main content
Associate
Apr 8, 2025 6:37 AM UTC
Question

Connector for Murata M.2 module Adapter to STM32 MPU (40-GPIO Pin Header)

Dear STMicroelectronics Community,

I hope this message finds you well.

We are currently working on integrating the Murata M.2 Wi-Fi module with an STM32 MPU platform(STM32MP157D-DK1). The STM32 board provides a 40-GPIO pin header interface, and the Murata module is mounted on an M.2 adapter.

We would like to inquire if there is any existing connector or adapter solution available that can interface the Murata M.2 adapter with the 40-GPIO pin header on the STM32 MPU, specifically supporting SDIO and UART lines.

Any guidance or recommendations on compatible hardware or reference designs would be greatly appreciated.

Thank you for your support.

Best regards,
[Adarsh Katiyar]
[engineer]
[acl DIGITAL]
[9651373221]

This topic has been closed for replies.