Skip to main content
Associate III
October 5, 2023
Question

Clarification requires on STM32MP157 timer peripheral clocks enable region

Hello

      We are using timer peripheral in STM32MP157 Cortex -A7 core 0 processor. In this, we enabled TIM2, TIM3, TIM4 in RCC APB1 peripheral enable for MPU set register, now we unable to use these timers (not getting interrupts) in Cortex -A7 core 0 processor. But we enabled these same timers in RCC APB1 peripheral enable for MCU set register, at this time getting interrupts in Cortex -A7 core 0 processor. 

      So, any reason these timers (TIM2, TIM3, TIM4) enables in MCU set register to use in Cortex -A7 core 0 processor. remaining all peripherals are works with enables same MPU set register. 

regards 

srikanth

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
October 5, 2023

Hi @Srikanth1 

Maybe related to low power mode of Cortex-A7 and value in RCC_MP_APB1LPENSETR.
TIMers on APB1 need AHB2 clock running to generate interrupts, which might be forced to be enabled when you use MCU register if Cortex-M4 is not in low power mode.
See also Reference Manual "Peripheral clock gating control" and "Bus matrix and bridges clock gating" sections.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent