Change u-boot kernel command line
- 2 replies
- 4276 views
Hello there,
I have a OSD32MP1-RED board based on stm32mp157c. Following the instructions How to create your own machine, I was able to compile the image. The problem happens when I try to boot from SD card with the generated image after load the boot loader and kernel, I got the error:
Waiting for root device /dev/mmcblk0p6...
After some research, I realized the mmcblk0p6 corresponds to eMMC memory in my board (but now this is empty). So, I have tried to modify the kernel's arguments adding in the config machine file the variable:
APPEND = "root=/dev/mmcblk1p6 rootwait rw console=ttySTM0,115200 init=/sbin/init firmware_class.path=/lib/firmware/"
However I get the same result, the generated image alway points to the mmcblk1p6 block. My question is:
What variable do you need to set or modify to change the parameters passed to kernel from u-boot?
I attached the log file generated for more details.
Thanks in advance for your support.