Skip to main content
RGlie.1
Associate II
October 26, 2020
Solved

change pin mux in TF-A build for i2c-bus i2c4

We would like to build the TF-A image with a different muxer setting

for i2c4. The usual setting is:

i2c4_pins_a: i2c4-0 {

   pins {

      pinmux = <STM32_PINMUX('Z', 4, AF6)>, /* I2C4_SCL */

      <STM32_PINMUX('Z', 5, AF6)>; /* I2C4_SDA */

      bias-disable;

      drive-open-drain;

      slew-rate = <0>;

   };

};

our setup:

i2c4_pins_a: i2c4-0 {

   pins {

      pinmux = <STM32_PINMUX('H', 11, AF6)>, /* I2C4_SCL */

      <STM32_PINMUX('H', 12, AF6)>; /* I2C4_SDA */

      bias-disable;

      drive-open-drain;

      slew-rate = <0>;

   };

};

If we use the changed pin muxing we get no signal output on those pins.

My question, is it possible to change the pin muxing

or is the muxing for I2C4 fixed for the TF-A build ?

This topic has been closed for replies.
RGlie.1
RGlie.1Best answer
Associate II
October 27, 2020

Hello Olivier,

after updating the TF-A firmware to version v2.2-r1.4 the problem

is solved.

I think the reason was the issue:

"GPIO clock not enabled in BL32"

thank you,

Ralf

2 replies

Olivier GALLIEN
ST Technical Moderator
October 26, 2020

​Hi @RGlie.1​ 

I suspect you are facing known GPIO clock issue in V2.0.

Cf https://community.st.com/s/question/0D53W00000JQ4z4SAD/stm32mp1-ecosystem-known-bugs-and-common-pitfalls

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
RGlie.1
RGlie.1AuthorBest answer
Associate II
October 27, 2020

Hello Olivier,

after updating the TF-A firmware to version v2.2-r1.4 the problem

is solved.

I think the reason was the issue:

"GPIO clock not enabled in BL32"

thank you,

Ralf