Skip to main content
Jzhua
Associate III
December 16, 2020
Question

Cannot set a time greater than 2038

Cannot set a time greater than 2038, whether in the console or the c program

This topic has been closed for replies.

4 replies

Fee
Associate II
December 16, 2020

Hi,

not a solution but additional information:

This is a known bug named the 'Year 2038 problem' due to using a 32Bit signed Integer to count the seconds since 1 January 1970. There is even a Wikipedia article for it: https://en.wikipedia.org/wiki/Year_2038_problem

It should be solved by serveral kernel patches (see here: https://lkml.org/lkml/2020/1/29/355?anz=web) which I don't know if they are backported to the ST provided kernel (never looked at it, maybe a ST employee / other community member knows it, a quick git log --grep y2038 showed some related commits). Also this post might help you: https://unix.stackexchange.com/questions/396373/bash-date-working-around-the-2038-bug-on-32bit-linux-system

Jzhua
JzhuaAuthor
Associate III
March 1, 2021

Does ST have specific instructions or patching plans for this issue, Our development underway and nearing completion, Considering that the device will continue to be sold and maintained for more than year 2038, hope to solve this problem before going on market

Uwe Bonnes
Chief
March 1, 2021

The hardware seem obvious to be capable of working after 2038 as it count second/minutes/hourds/days/month/ years. Check and rewrite the software. Try to set the date direct in the registers.

Jzhua
JzhuaAuthor
Associate III
March 2, 2021

I think this is not a good way. In the Linux ecosystem, there are a large number of middlewares that use the libc interface instead of registers to get the system time. This is neither a standard implementation, nor the ability of small organizations to modify so many software, so I still hope that ST can solve the problem. I found that this problem is common in 32-bit systems. The kernel seems to have completely fixed this problem after 5.6. I don’t know if ST has plans to patch the current version.