Skip to main content
PS.2
Associate III
October 4, 2022
Question

Can we use STM32MP157A-EV1 image for flashing our custom STM32MP1 based board ?

Hi,

I tried burning my STM32MP1 board with existing "FlashLayout_emmc_stm32mp157a-ev1-trusted.tsv" file but it throws following error -

Error: TSV files are only supported for STM32MP

I'm using onboard eMMC (From Kioxia) and STM32MP157AAD3 chip from ST. I have attached snapshot of log. and I'm extremely in need of support

user@user:~/STM32MPU-Ecosystem-v4.0.0/Starter-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/images/stm32mp1$ STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_emmc_stm32mp157a-ev1-trusted.tsv 
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.11.0 
 -------------------------------------------------------------------
 
 
 
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 0019002C3431511733353431
DFU protocol: 1.1
Board : --
Device ID : 0x0500
Device name : STM32MP1
Device type : MPU
Revision ID : -- 
Device CPU : Cortex-A7
 
Start Embedded Flashing service
 
 
 
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157a-ev1-usb.stm32
 File : tf-a-stm32mp157a-ev1-usb.stm32
 Size : 220.82 KB 
 Partition ID : 0x01 
 
Download in Progress:
[==================================================] 100% 
 
File download complete
Time elapsed during download operation: 00:00:01.150
 
RUNNING Program ... 
 PartID: :0x01 
 
 
Error: Start operation failed at partition 0x01
Error: TSV flashing service failed
user@user:~/STM32MPU-Ecosystem-v4.0.0/Starter-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/images/stm32mp1$ STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_emmc_stm32mp157a-ev1-trusted.tsv 
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.11.0 
 -------------------------------------------------------------------
 
 
 
USB speed : High Speed (480MBit/s)
Manuf. ID : 
Product ID : 
SN : 
DFU protocol: 1.1
Board : --
IAP
Error: TSV files are only supported for STM32MP

@PatrickF​ 

@Community member​ 

@OlivierK​ 

@Kevin HUBER​ 

This topic has been closed for replies.

2 replies

PS.2
PS.2Author
Associate III
October 11, 2022

Hello Team ST.

I'm using THGBMUG6C1LBAIL (eMMC from Kioxia JEDEC 5.1). Will it be the reason for above issue ?

Thank you.

@Community member​ 

PatrickF
ST Employee
November 16, 2022

Hi @PS.2​ 

sorry for late answer.

Did you progress on that issue ?

Would be good to have the board UART console output.

Btw, flashing using EV1 binaries would mean that your board have exactly same HW for TF-A and uBoot usage (e.g. same pins for same functions, uses STPMIC1A, same DDR3L, same UART for console, same I2C for STPMIC1, etc..).

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent