Skip to main content
MÇerçi
Associate III
November 25, 2020
Solved

Can't run gtk_hello_world example on STM32MP157A

Hi, i dont know if it is a stupid question or not but anyways, I was following the STM32MP157A-DK2 tutorial for developing on ARM Cortex A7

i maked the example given for hello_world.c with given makefike. It works fine on my linux pc but the borad i cant run it on the board. it gives this error every time.

@@@@�0hello_world: line 1: can't open @8
 0
 ��: no such file
./gtk_hello_world: line 1: ./gtk_hello_world: line 6: : not found
./gtk_hello_world: line 1: �qXX���+�l��: not found
ELF: not found
./gtk_hello_world: line 1: ?h?p?x?�?��?: not found
./gtk_hello_world: line 6: ./gtk_hello_world: line 2: �?
 �?
 �?�?�?�?��H�H��/H��t��H���5�/��%�h���������h���������h���������h��������h��������h��������h��������h��q��������a������h: not found
can't open-�8?8@0
 @00*@0�: no such file./gtk_hello_world: line 3: ��A������h
 ��1������h
��������h��������h�����������%�.D����%.D����%�-D����%�-D����%�-D����%�-D����%�-D����%�-D����%�-D����%�-D����%�-D����%�-D����%�-D����%�-D����%�-D����%�-D����%�-D�H�=3�z-��H�=�-H��-H9�tH�V-H��t: File name too long
 
./gtk_hello_world: line 1: can't open K: no such file
./gtk_hello_world: line 1: E�: not found
./gtk_hello_world: line 6: : not found
./gtk_hello_world: line 6: �: not found

it always gives me error i cant even run just a printf line:

#include <gtk/gtk.h>
int main ()
{
	printf("Hello_World!!");
}

it gives

root@stm32mp1:/usr/local# ./gtk_hello_world
./gtk_hello_world: line 1: syntax error: unexpected "("

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
November 25, 2020

Hi @Mustafa Çerçi​ 

it's not only a matter of installation of SDK but source the env prior to make

You should get :

PC $> echo $CROSS_COMPILE

arm-ostl-linux-gnueabi-

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

8 replies

Olivier GALLIEN
ST Technical Moderator
November 25, 2020

Hi @Mustafa Çerçi​ 

Same executable can not work both on your linux station and on Target

If working well on your station I suspect you forget, or not properly, load the SDK prior to call make command in order to cross-compile for MP1.

Double check your procedure.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MÇerçi
MÇerçiAuthor
Associate III
November 25, 2020

Thanks for the fast answer, I installed SDK before i can do it again, now deleted every file now started installing again. After i finish that i will try to build again

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
November 25, 2020

Hi @Mustafa Çerçi​ 

it's not only a matter of installation of SDK but source the env prior to make

You should get :

PC $> echo $CROSS_COMPILE

arm-ostl-linux-gnueabi-

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.