Skip to main content
Lead
Jun 7, 2025 11:43 PM UTC
Solved

Can I use the same USB hub schematic from STM32MP1 for STM32MP2?

In STM32MP1, there is an USB hub for 4 USB-A connectors. The hub is Microchip USB2514B. Were 4 means "4 ports".

In STM32MP2, there is an USB too, for 2 USB-A connectors. The hub is Microchip USB2412B. Were 2 means "2 ports".

According to AN5489, it says at 8.13 " Multiple hi-speed USB hosts using an external USB hub component is not described here.". So is that an answer for "yes, it's possible to use USB 2514B with STM32MP2"? 

This topic has been closed for replies.
PatrickF
PatrickFBest answer
ST Employee
Jun 9, 2025 11:46 AM UTC

Hi @DMårt ,

 

I see no blocking point to use whatever embedded HUB (like USB 2514B or else) on STM32MP2 platform, connected to USBH.

Just need to align Device Tree to the right external device in case there is SW configuration needs (e.g. I2C bus, reset signal, etc...).

Regards,

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent

1 reply

PatrickF
PatrickFBest answer
ST Employee
Jun 9, 2025 11:46 AM UTC

Hi @DMårt ,

 

I see no blocking point to use whatever embedded HUB (like USB 2514B or else) on STM32MP2 platform, connected to USBH.

Just need to align Device Tree to the right external device in case there is SW configuration needs (e.g. I2C bus, reset signal, etc...).

Regards,

 

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent