Skip to main content
vlacr.11
Associate II
January 31, 2022
Solved

Bug report: STM32CubeProgrammer flash failure on STM32MP1

On my Ubuntu 20.04, Flashing of STM32MP157C-DK2 with STMCubeProgrammer fails with the following error I easily reproduced using the scripts:

$ STM32_Programmer.sh -c port=usb1 -w FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.9.0 
 -------------------------------------------------------------------
 
 
 
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 002C002E3338511134383330
FW version : 0x0110
Board : --
Device ID : 0x0500
Device name : STM32MP1
Device type : MPU
Revision ID : -- 
Device CPU : Cortex-A7
 
 
Start Embedded Flashing service
 
Error: File does not exist: /users/vincent/Documents/03_DEV/STM32MP1/en.FLASH-stm32mp1-openstlinux-5-10-dunfell-mp1-21-11-17_tar_v3.1.0/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/images/stm32mp1/flashlayout_st-image-weston/trusted/arm-trusted-firmware/tf-a-stm32mp157c-dk2-usb.stm32
Error: TSV flashing service failed

Indeed, the programmer is looking at a path which does not match with current filesystem.

I have got this errors for all the files the programmer was looking for. I have solved it by adding to symbolic links (instead of moving directories). For example:

0 [30 janv.-16:09:33] vincent@colin:~/Documents/03_DEV/STM32MP1/en.FLASH-stm32mp1-openstlinux-5-10-dunfell-mp1-21-11-17_tar_v3.1.0/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/images/stm32mp1/flashlayout_st-image-weston/trusted
$ ln -s ../../arm-trusted-firmware/ .

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
January 31, 2022

Hi @vlacr.1​ ,

tsv file are built with related path to binaries from "/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/images/stm32mp1"

You have to run CubeProg from this path and use CLI command :

vincent@colin: cd ~/Documents/03_DEV/STM32MP1/en.FLASH-stm32mp1-openstlinux-5-10-dunfell-mp1-21-11-17_tar_v3.1.0/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/images/stm32mp1
vincent@colin: STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

3 replies

Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
January 31, 2022

Hi @vlacr.1​ ,

tsv file are built with related path to binaries from "/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/images/stm32mp1"

You have to run CubeProg from this path and use CLI command :

vincent@colin: cd ~/Documents/03_DEV/STM32MP1/en.FLASH-stm32mp1-openstlinux-5-10-dunfell-mp1-21-11-17_tar_v3.1.0/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/images/stm32mp1
vincent@colin: STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
vlacr.11
vlacr.11Author
Associate II
February 8, 2022

Hello @Community member​ ,

Ok understood. Thanks for your answer. I think we can close this ticket.

Best Regards,

Vincent

Olivier GALLIEN
ST Technical Moderator
February 9, 2022

Hi @vlacr.1​ ,

Thanks for feedback ! :smiling_face_with_smiling_eyes:

In this Q&A forum, the only and best way to close a conversation is to mark as "Best answer" the answer which help you.

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.