Skip to main content
Associate
Jan 30, 2025 7:21 PM UTC
Question

Bringing up STM32MP257 & Debug

We have built a SBC using the 257EV as a reference in Altium. We are trying to use debug. We have created a ST14 connector to connect to a STLink3 using UART 2 as the debug serial port.

Is this possible, and should we use SWD or JTAG to debug the processor.

At present we are stuck at a flashing red led1. At present the DDR & GPU supplies haven't started on the PMIC, the remaining supplies are all present, as is the HSE clock.

Any thoughts would be appreciated.

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
Jan 31, 2025 7:26 AM UTC

Hi,

UART is a kind of minimum to allows console log.

SWD or JTAG is nice to have in case you want to debug low level SW (Cortex-M33, Linux driver, TF-A, etc...).

Have you build a customized image for your board (e.g. using Yocto) ?

Did you try to populate this image to your board ? Need at minimum USB3DRD device connection to a PC.
See how it is done using STM32MP257F-EV1: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP2_boards/STM32MP257x-EV1/Let%27s_start/Populate_the_target_and_boot_the_image
flashing red led at 5Hz mean the bootROM is waiting for a USB DFU connection (for flashload). Could be because no valid flash content detected or Boot pins are set to 0b0000 or 0b1111.

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent