Skip to main content
MThom.5
Visitor II
July 26, 2019
Question

Bluetooth not working on STM32MP157C-DK2 board ("basic" image)

I'm trying to build an image for the STM32MP157C-DK2 board using the standard unmodified OpenSTLinux yocto build.

The build is successful and the image boots fine, but Bluetooth does not work with the basic image (it works with the trusted image).

Using a scope, I noticed that BT_REG_ON (on TP29) is driven low, which turns off the bluetooth part of the chip.

I suspect that the device tree is parsed differently depending on the bootloader used (the device tree itself is identical to the one that is preloaded on the provided SDCard).

Build Configuration:
BB_VERSION = "1.40.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-19.04"
TARGET_SYS = "arm-openstlinux_weston-linux-gnueabi"
MACHINE = "stm32mp1"
DISTRO = "openstlinux-weston"
DISTRO_VERSION = "2.6-snapshot-20190726"
TUNE_FEATURES = "arm armv7ve vfp thumb neon vfpv4 callconvention-hard cortexa7"
TARGET_FPU = "hard"
DISTRO_CODENAME = "thud"
ACCEPT_EULA_stm32mp1 = "1"
GCCVERSION = "8.%"
PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"
meta-oe 
meta-gnome 
meta-xfce 
meta-initramfs 
meta-multimedia 
meta-networking 
meta-webserver 
meta-filesystems 
meta-perl 
meta-python = "HEAD:f1511d254632a34c1deb51f4bf8b8c21e7423f51"
meta-st-stm32mp = "HEAD:dcc955d6992cc46ce07440caaa5a17942776bbe6"
meta-qt5 = "HEAD:fd1f0f47312e7ee80e5ca65b8b2992cb068b1656"
meta-st-openstlinux = "HEAD:4e36cf0c7c7bdb24700a990f73afcda84cdcf0cf"
meta = "HEAD:f0394e80a37f1da47042a1aa0487594f390603f9"

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
July 26, 2019

Hello,

we recommend to use 'trusted boot' chain, which provide you full feature availability.

see https://wiki.st.com/stm32mpu/wiki/Boot_chains_overview#Overview

Note: The basic boot chain is not promoted by STMicroelectronics to make products, it is only provided to support the DDR Tuning Tool and the U-Boot developments.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent