Skip to main content
Ara.1
Associate III
February 25, 2022
Question

Audio play different bitrate test

i am using gst-play-1.0 for testing different bitrate audio play, found that 44.1 kbps, 22.050 kbps were not working but 48kbps mp3 works neatly without noise

Please let me know if i miss anything, i am using I2S1 to derive the base MCLK and feed to codec

log:

gst-play-1.0  /run/media/mmcblk0p1/AudioFiles/test.wav 

playing 22.05kbps--- (256*22.05k) = 5644800

Press 'k' to see a list of keyboard shortcuts.

Now playing /run/media/sda1/AudioFiles/BabyElephantWalk60.wav

[ 1164.185749] st,stm32-i2s 44004000.audio-controller: Error -16 setting i2sclk parent clock 5644800

playing 44.1kbps--- (256*44.1k) = 11289600

Now playing /run/media/sda1/AudioFiles/Railroad.mp3

[ 1523.259773] st,stm32-i2s 44004000.audio-controller: Error -16 setting i2sclk parent clock 11289600 -309581440 -309581312

[ 1523.269268] asoc-audio-graph-card sound@0: ASoC: machine hw_params failed: -16

ERROR Could not get/set settings from/on resource. for file:///run/media/sda1/AudioFiles/Railroad.mp3

ERROR debug information: ../../../gst-plugins-base-1.14.4/ext/alsa/gstalsasink.c(617): set_hwparams (): /GstPlayBin:playbin/GstPlaySink:playsink/GstBin:abin/GstBin:bin0/GstAlsaSink:alsasink0:

Unable to set hw params for playback: Device or resource busy

Reached end of play list.

This topic has been closed for replies.

9 replies

Ara.1
Ara.1Author
Associate III
February 25, 2022

Hi any one came across this ?

Ara.1
Ara.1Author
Associate III
March 2, 2022

Hi Any body can able to test from eval board ?

Ara.1
Ara.1Author
Associate III
March 2, 2022

44.1kbs file

Ara.1
Ara.1Author
Associate III
March 2, 2022
Kevin HUBER
ST Employee
March 3, 2022

Hello @Ara.1​ ,

Thank you for the files.

On my side, the two files are working well with the stm32mp157f-dk2 and a headset plugged on the jack plug.

I am using the internal codec with the starter package v3.1.

root@stm32mp1:~# gst-play-1.0 /usr/local/Test_44100.mp3 
Press 'k' to see a list of keyboard shortcuts.
Now playing /usr/local/Test_44100.mp3
Redistribute latency...
0:02:00.5 / 0:05:40.9 
root@stm32mp1:~# gst-play-1.0 /usr/local/Test_22050.mp3 
Press 'k' to see a list of keyboard shortcuts.
Now playing /usr/local/Test_22050.mp3
Redistribute latency...
0:00:05.1 / 0:00:05.1 
Reached end of play list.
 

In your log, you have a lot of error that I didn't have. I think it can explains your errors.

-------------

Which version of ecosystem do you use?

Can I have your DTS file and the complete boot log of your board please?

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Ara.1
Ara.1Author
Associate III
March 3, 2022

Hi Kevin,

Thanks for replay

i do see two audio interface

SAI

I2S2

as per board you mentioned,

in command line can you run following command:

root@stm32mp1:~# aplay -l

may you try play gstplay with specific HW or instance where I2S2 runs

 root@stm32mp1:~# speaker-test --device hw:0,2 --rate 44100 --channels 2 --format S16_LE --test wav

Kevin HUBER
ST Employee
March 10, 2022

Hello @Ara.1​ ,

I am now on a board 157C-DK2 and it works well. Below the results of the two commands that you asked for:

root@stm32mp1:~# aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: STM32MP15DK [STM32MP15-DK], device 0: 4400b004.audio-controller-cs42l51-hifi cs42l51-hifi-0 [4400b004.audio-controller-cs42l51-hifi cs42l51-hifi-0]
 Subdevices: 1/1
 Subdevice #0: subdevice #0
card 0: STM32MP15DK [STM32MP15-DK], device 2: 4000b000.audio-controller-i2s-hifi i2s-hifi-2 [4000b000.audio-controller-i2s-hifi i2s-hifi-2]
 Subdevices: 1/1
 Subdevice #0: subdevice #0
root@stm32mp1:~# speaker-test --device hw:0,2 --rate 44100 --channels 2 --format S16_LE --test wav
 
speaker-test 1.2.1
 
Playback device is hw:0,2
Stream parameters are 44100Hz, S16_LE, 2 channels
WAV file(s)
Rate set to 44100Hz (requested 44100Hz)
Buffer size range from 512 to 8192
Period size range from 256 to 4096
Using max buffer size 8192
Periods = 4
was set period_size = 2048
was set buffer_size = 8192
Sample rate doesn't match (48000) for /usr/share/sounds/alsa/Front_Left.wav
root@stm32mp1:~# speaker-test --device hw:0,2 --rate 48000 --channels 2 --format S16_LE --test wav
 
speaker-test 1.2.1
 
Playback device is hw:0,2
Stream parameters are 48000Hz, S16_LE, 2 channels
WAV file(s)
Rate set to 48000Hz (requested 48000Hz)
Buffer size range from 512 to 8192
Period size range from 256 to 4096
Using max buffer size 8192
Periods = 4
was set period_size = 2048
was set buffer_size = 8192
 0 - Front Left
 1 - Front Right
Time per period = 2.863147
 0 - Front Left
 1 - Front Right

-------------------------------------

Please can you answer to these questions:

  • Which version of ecosystem do you use? (Version of linux)
  • Can I have your DTB file and the complete boot log of your board please?
Please let me know if i miss anything, i am using I2S1 to derive the base MCLK and feed to codec

Which kind of board are you using please? I saw in other topics that you were using a custom board, but is it the case here?

And can you please also send me the traces of the command:

root@stm32mp1:~# aplay -l

and:

root@stm32mp1:~# pactl list cards

Regards,

Kévin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Ara.1
Ara.1Author
Associate III
March 25, 2022

i have the stm32m157C-DK2 board now, i too seen all the bit rates are working, but the mclk is floating , i did a grep on mclk on /sys/debug/clk_summary i do not see any spix_mclk getting created, whic means that i2s2 is slave, and codec is master in the HDMI I2S2,

please correct me if am wrong

Kevin HUBER
ST Employee
April 19, 2022

Hello @Ara.1​ ,

As already asked twice I will need your DTS file and your complete DTB to help you.

Can you send me your complete bootlog too please?

I modified my DTS of the DK2 to have the codec CS42L51 as a consumer of SAI2A master clock and it works also.

I would like to have your DTS and DTB as asked above to reproduce a configuration like yours with the i2s2 that feed the codec and reproduce the problem.

In your first log, you had a lot of error i2sclk that looks like error of configuration in the DTS.

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.