Skip to main content
SMang.1
Associate II
October 6, 2020
Question

APB5 access in Engineering mode

Hi,

Can I access APB5 bus in engineering mode to run I2C4 with I2C4_SCL = PZ4, I2C4_SCL = PZ5?

This topic has been closed for replies.

3 replies

PatrickF
ST Employee
October 6, 2020

Yes, in engineering mode, RCC is in non-secure mode, as well as all IPs secured by ETZPC (except secrets like ROM or some OTPs which are still protected). Except for memory map restrictions, this stand for Cortex-A7 and Cortex-M4.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
SMang.1
SMang.1Author
Associate II
October 6, 2020

Thanks @PatrickF​ .

Just to confirm, the clock for APB5 is derived from what core?

PatrickF
ST Employee
October 6, 2020

APB5 (pclk5) root clock usually come from PLL2 (AXI clock) with dedicated sub-dividers.

See product RefMan (e.g. RM0436 for STM32MP157), "Core and busses clock generation" in RCC section.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent