Skip to main content
This topic has been closed for replies.

5 replies

Olivier GALLIEN
ST Technical Moderator
December 3, 2019

Hi @moredatalesscenter​ 

Android does not fit to DK2 because there is not enough DDR ( 1GB required) .

Guideline to install Android on target is there :

https://wiki.st.com/stm32mpu/wiki/How_to_populate_boards_for_Android

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
moredatalesscenter
Associate III
December 3, 2019

Ah. The board features suggest it's 4 Gbit DDR3L, 16 bits.

Olivier GALLIEN
ST Technical Moderator
December 3, 2019

Indeed ..which mean 512MBytes. ;)

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
moredatalesscenter
Associate III
December 5, 2019

Can packages be selectively removed to create a barebones distribution that will fit into 0.5GB?

Nicolas L
ST Employee
December 5, 2019

Android from AOSP can work with 512MBytes but with an impact on the overall performance (swap has a huge impact).

It's then required to limit the memory usage to the maximum:

1- limit the display resolution on the device

2- limit the number of packages started (remove all unnecessary packages which can means patching the system server to avoid starting them (ex: Telecom))

3- applications (packages) including the Launcher shall be developed considering memory usage (no animation, simple layouts (ex: use ConstrainLayout), avoid too much activity swap...)

At the end, it depends on the kind of device targeted (ex: wear device with small screen can work easily with 512MBytes DDR)