Skip to main content
Senior
Jan 20, 2025 6:23 AM UTC
Solved

AN5861 - Power rating for R4 (8R2)

Is there a recommended minimum SMT package size and power rating for resistor R4 (8R2) please?

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jan 20, 2025 7:46 AM UTC

R4 is only connected to GND by Q1 for a very short time, defined by the monoflop U1 with R3/C3, so that the heating of R4 is almost negligible depending on its dimensioning. With the approx. 0.4ms (100k, 5.6nF) from AN5861, a resistor size of 0805 is certainly sufficient.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Jan 20, 2025 7:46 AM UTC

R4 is only connected to GND by Q1 for a very short time, defined by the monoflop U1 with R3/C3, so that the heating of R4 is almost negligible depending on its dimensioning. With the approx. 0.4ms (100k, 5.6nF) from AN5861, a resistor size of 0805 is certainly sufficient.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
alwAuthor
Senior
Jan 20, 2025 8:22 AM UTC

Hi Peter,

Thanks very much.

Kind regards,

Al