Skip to main content
SAman.1
Associate III
May 27, 2021 11:59 AM UTC
Question

Why does my Transmition is not complete.

Hello on my serdev when i set it up the transmition complete is not set:

stm32-usart 4000f000.serial: transmission complete not set

I configurated my device tree like this:

&usart3 {

compatible = "st,stm32-uart", "st,stm32f7-uart", "st,stm32h7-uart";

pinctrl-names = "default", "sleep", "idle";

pinctrl-0 = <&usart3_pins_b>;

pinctrl-1 = <&usart3_sleep_pins_b>;

pinctrl-2 = <&usart3_idle_pins_b>;

uart-has-rtscts;

status = "okay";

ethernet {

compatible = "st,stm32_usart_net";

local-mac-address = [ A0 B0 C0 D0 E0 F0 ];

current-speed = <38400>;

};

};

So in my system it shows up like this:

/sys/devices/platform/soc/4000f000.serial/serial0/serial0-0

  • driver
  • modalias
  • of_node
  • power
  • subsystem
  • uevent

The probe methode of my serdev_device_driver looks like this:

struct stmuart *stm;

u32 speed = 115200;

int ret;

stm = devm_kzalloc(&serdev->dev, sizeof(*stm), GFP_KERNEL);

stm->serdev = serdev;

spin_lock_init(&stm->lock);

INIT_WORK(&stm->tx_work, stmuart_transmit);

serdev_device_set_drvdata(serdev, stm);

serdev_device_set_client_ops(serdev, &stm_serdev_ops);

ret = serdev_device_open(serdev);

if (ret) {

dev_err(&serdev->dev, "Unable to open device\n");

goto free;

}

speed = serdev_device_set_baudrate(serdev, speed);

dev_info(&serdev->dev, "Using baudrate: %u\n", speed);

serdev_device_set_flow_control(serdev, true);

return 0;

My kernel shows me the log when i call the "serdev_device_open" methode. But i can not find something to set options to the serdev_device to avoid it. I looked some other examples and there i also did not find a setting for the device tree. My Kernel is on version 5.4

This topic has been closed for replies.

9 replies

SAman.1
SAman.1Author
Associate III
May 31, 2021 8:54 AM UTC

Sorry that i tag you but do you have an idea

@Community member​ 

SAman.1
SAman.1Author
Associate III
May 31, 2021 2:08 PM UTC

I tried the kernel version 5.10 but the same ressult.

SAman.1
SAman.1Author
Associate III
Jun 1, 2021 7:25 PM UTC

I figuret the mistake out and i was able to make a loopback module but now i get this exception:

[33168.807576] ------------[ cut here ]------------

[33168.812054] WARNING: CPU: 0 PID: 1392 at /home/gonzo/projects/SerdevTest/usartHci.c:45 stm_tty_receive+0x4c/0x8c [usartHci]

[33168.823255] Modules linked in: usartHci(OE) cfg80211 snd_soc_cs42l51 snd_soc_hdmi_codec snd_soc_stm32_sai_sub snd_soc_audio_graph_card snd_soc_simple_card_utils snd_soc_stm32_i2s snd_soc_core usb_f_rndis u_ether snd_pcm_dmaengine libcomposite snd_pcm stusb160x typec snd_timer snd stm32_hash stm32_crc32 crypto_engine snd_soc_stm32_sai stm32_cec soundcore sch_fq_codel ipv6 [last unloaded: usartHci]

[33168.858431] CPU: 0 PID: 1392 Comm: kworker/u4:1 Tainted: G    W OE   5.10.10 #2

[33168.866254] Hardware name: STM32 (Device Tree Support)

[33168.871406] Workqueue: events_unbound flush_to_ldisc

[33168.876377] [<c0110824>] (unwind_backtrace) from [<c010c4e0>] (show_stack+0x10/0x14)

[33168.884110] [<c010c4e0>] (show_stack) from [<c0b8319c>] (dump_stack+0xb8/0xcc)

[33168.891335] [<c0b8319c>] (dump_stack) from [<c01249c0>] (__warn+0xec/0x104)

[33168.898295] [<c01249c0>] (__warn) from [<c0b7e65c>] (warn_slowpath_fmt+0x64/0xc4)

[33168.905786] [<c0b7e65c>] (warn_slowpath_fmt) from [<bf1360ec>] (stm_tty_receive+0x4c/0x8c [usartHci])

[33168.915014] [<bf1360ec>] (stm_tty_receive [usartHci]) from [<c06b5574>] (ttyport_receive_buf+0x50/0xf4)

[33168.924410] [<c06b5574>] (ttyport_receive_buf) from [<c0693ef4>] (flush_to_ldisc+0x8c/0xe0)

[33168.932765] [<c0693ef4>] (flush_to_ldisc) from [<c0141798>] (process_one_work+0x1dc/0x59c)

[33168.941032] [<c0141798>] (process_one_work) from [<c0141ba4>] (worker_thread+0x4c/0x520)

[33168.949128] [<c0141ba4>] (worker_thread) from [<c014818c>] (kthread+0x144/0x180)

[33168.956526] [<c014818c>] (kthread) from [<c0100148>] (ret_from_fork+0x14/0x2c)

[33168.963741] Exception stack(0xc3e1dfb0 to 0xc3e1dff8)

[33168.968793] dfa0:                   00000000 00000000 00000000 00000000

[33168.976976] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[33168.985155] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000

[33168.991879] ---[ end trace 29e46253976aa845 ]---

it only pops up when i sent the data when i just print what i recive i get no error,

my loopack looks like this:

static int

stm_tty_receive(struct serdev_device *serdev, const unsigned char *data,

size_t count)

{

  struct stmuart *stm = serdev_device_get_drvdata(serdev);

int len;

  u8 *pos;

   

  spin_lock(&stm->lock);

   

  WARN_ON(stm->tx_left);

  pos = stm->tx_buffer;

   

  len = serdev_device_write_buf(serdev,

   data, count);

  stm->tx_left = (pos - stm->tx_buffer) - len;

stm->tx_head = stm->tx_buffer + len;

     

  spin_unlock(&stm->lock);

return len;

}

SAman.1
SAman.1Author
Associate III
Jun 1, 2021 7:34 PM UTC

The issue was that my device tree was not setup corectly thats why i had this issue before

Olivier GALLIEN
ST Technical Moderator
Jun 2, 2021 9:04 AM UTC

Hi @SAman.1​ ,

Sorry to come late in the thread.

Seems you figure out by yourself the issue.

Could you elaborate further "my device tree was not setup correctly" ?

Which node/properties exactly ?

This may help other members and us in ST to better know where was the trap.

Thanks,

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SAman.1
SAman.1Author
Associate III
Jun 2, 2021 1:55 PM UTC

I needed to enable it on the stm32mp151.dtsi and not in the stm32mp15xx-dkx.dtsi.

But i have a new question when enable serdev_device_set_flow_control(serdev, true); it is not sending and the CTS and RTS not get changed. do i need to enable more to get hardware flow control on a serdev.

Olivier GALLIEN
ST Technical Moderator
Jun 3, 2021 9:09 PM UTC

Hi @SAman.1​ 

Maybe this old post can help to setup HW Flow control

https://community.st.com/s/question/0D53W0000037Pi0SAE/how-to-enable-hardware-flow-control-rs485

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SAman.1
SAman.1Author
Associate III
Jun 4, 2021 6:57 AM UTC

Hi I saw that post already but it did not helped me because I wanted to use it from my serial device bus.

SAman.1
SAman.1Author
Associate III
Jun 4, 2021 4:11 PM UTC

I am also not able to change my CTS or RTS pin with the serdev_device_set_tiocm methode.