Skip to main content
Associate II
Feb 5, 2026 10:32 AM UTC
Question

Which cores are the STLINK-V3EC can support, does support cortex A35/A7 core?

Recently,I test STM32MP2 with STM32MP257F-EV1 board.
I want to debug A35 core with STLINKV3 that on the STM32MP257F-EV1 board,does it support ?
And which cores are the STLINK-V3EC can support,except cortex M.

2 replies

PatrickF
ST Employee
Feb 5, 2026 1:05 PM UTC
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Da_VinciAuthor
Associate II
Feb 5, 2026 1:28 PM UTC

Hi,Patrick,

I know that STLINKV3EC on the STM32MP257F-EV1 board can debug the M33 core, now I want to debug the cortex A35 core by it, but when I choose the A35 core in CubeIDE, it reminds me that this probe does not support.

the second question,  after choose the M33 core in CubeIDE debug configuration window, the STLINKV3 could be find in this window, and get the SN of STLINKV3, but when back to main window, after click debug button, the IDE pop-up a window say that can not detect the STLINK.

Using the 3rd party debug probes, the M33 and A35 core all can be debugged normally by SWD.