Skip to main content
lsalv
Associate
Mar 5, 2019 2:28 PM UTC
Solved

Where is the fw_cortex_m4.sh. in a STM32MP157C DK2 Yocto build?

Hi all,

yesterday I just booted the amazing STM32MP1 DK2 device with a brand new Yocto build (st-image-weston). Can't find the fw_cortex_m4.sh . Is that available just in the STM32CubeMP1_Package or maybe I need to add another layer and build for another target?

This topic has been closed for replies.
GwenaelT
GwenaelTBest answer
Visitor II
Mar 6, 2019 4:35 PM UTC

You can find more informations about boot modes here :

https://wiki.st.com/stm32mpu/index.php/STM32CubeMP1_Package#Select_boot_mode_for_m4_examples

Otherwise the M4 firmware are also built in yocto image. You can find more informations here :

https://wiki.st.com/stm32mpu/index.php/STM32CubeMP1_Package#Introduction_to_m4projects_recipe

4 replies

Olivier GALLIEN
ST Technical Moderator
Mar 5, 2019 2:51 PM UTC

Hi,

fw_cortex_m4.sh is specific to an M4 firmware application.

You can find one in each Cube-M4-examples pre-load in the image here :

root@stm32mp1:/usr/local/Cube-M4-examples/STM32MP157C-DK2/Examples/

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
lsalv
lsalvAuthor
Associate
Mar 5, 2019 3:28 PM UTC

I think I'm missing something.

I build and flash the yocto OpenSTLinux then I was following this doc...

https://wiki.st.com/stm32mpu/index.php/OpenSTLinux_directory_structure

But now that I booted with a terminal on /dev/ttyACM0 I got this ...

Select the boot mode

1:   stm32mp157c-dk2-sdcard

2:   stm32mp157c-dk2-a7-examples-sdcard

3:   stm32mp157c-dk2-m4-examples-sdcard

And run some of them:

root@stm32mp1:/usr/local/Cube-M4-examples/STM32MP157C-DK2#

But means that those are built an pushed as separate images?

I can't find event the M4 images, like the OpenAMP_TTY_echo.elf, it's on the board but no in the Yocto build directory.

I'm sure I didn't get where this data comes from :D

GwenaelT
GwenaelTBest answer
Visitor II
Mar 6, 2019 4:35 PM UTC

You can find more informations about boot modes here :

https://wiki.st.com/stm32mpu/index.php/STM32CubeMP1_Package#Select_boot_mode_for_m4_examples

Otherwise the M4 firmware are also built in yocto image. You can find more informations here :

https://wiki.st.com/stm32mpu/index.php/STM32CubeMP1_Package#Introduction_to_m4projects_recipe

lsalv
lsalvAuthor
Associate
Mar 6, 2019 4:53 PM UTC

Thank you very much.

This doc was exactly what I was looking for.

Thank you!