Skip to main content
MWors.1
Associate II
Jan 5, 2021 7:48 AM UTC
Question

What is the proper procedure to secure a bootloader build for the DK1?

I've attempted to build my own u-boot image based on the trusted defconfig and a dk1 device tree, i.e.

$ make stm32mp15_basic_defconfig
$ make DEVICE_TREE=stm32mp157a-dk1 all

The build worked successfully, however when I attempted to use the `u-boot.stm32` image it failed to flash/boot. Getting the older fsbl working to flash my image into the ssbl ended up with failing messages:

stm32_smc: Failed to exec in secure mode (err = -3)
stm32_smc: Failed to exec in secure mode (err = -3)
stm32_smc: Failed to exec in secure mode (err = -3)
stm32_smc: Failed to exec in secure mode (err = -3)
stpmic1_read: failed to read register 0x22 : -110stpmic1_read: failed to read register 0x22 : -110stpmic1_read: failed to read register 0x22 : -110stpmic1_read: failed to read register 0x22 : -110Can't enable vdda-supply: -110
stpmic1_read: failed to read register 0x22 : -110stpmic1_read: failed to read register 0x22 : -110stpmic1_read: failed to read register 0x22 : -110stpmic1_read: failed to read register 0x22 : -110Can't enable vdda-supply: -110

Clearly the build wasn't secure so it couldn't be booted. I attempted to fix this via the STM32MP_KeyGen_CLI.exe and STM32MP_SigningTool_CLI.exe. I generated keys based on a test password that I created, then signed my u-boot image and flashed that instead.

After flashing, I attempted to boot and ran into a different error:

NFO: PMIC version = 0x10
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.2-r2.0(debug):v2.2-dirty
NOTICE: BL2: Built : 13:36:23, Oct 22 2019
INFO: Using crypto library 'stm32_crypto_lib'
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2 runs SP_MIN setup
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffeb000
INFO: Image id=4 loaded: 0x2ffeb000 - 0x2ffff000
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: STM32 Image size : 810794
INFO: Image id=5 loaded: 0xc0100000 - 0xc01c5f2a
INFO: Check signature on Open device

Basically the DK hangs here at "check signature". I'm guessing because I generated it incorrectly somehow, or it was looking for something specific.

Are there any instructions on the correct way to "sign" a u-boot image to be used by the DK1?

Thanks.

-Mike

This topic has been closed for replies.

9 replies

Olivier GALLIEN
ST Technical Moderator
Jan 5, 2021 8:58 AM UTC

Hi @MWors.1​ ,

If not already done I advise you to read https://wiki.st.com/stm32mpu/wiki/STM32MP15_secure_boot

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MWors.1
MWors.1Author
Associate II
Jan 7, 2021 2:38 PM UTC

@Community member​ Thanks for your response.

So if I'm reading this page correctly, the DK1, which has a STM32MP157A, can't actually do secure boot.

Cortex-A7 Cortex-M4 GPU Display CAN

STM32MP157 Dual Yes Yes TFT/DSI Yes

Security Cortex-A7 frequency

STM32MP15xA Basic 650 MHz[2]

Does this mean u-boot images for it should be created with the "basic" defconfig instead of the "trusted" one?

-Mike

Olivier GALLIEN
ST Technical Moderator
Jan 7, 2021 2:44 PM UTC

Hi @MWors.1​ ,

Yes you are right STM32MP15xA do not support secure boot.

From ecosystem V2.x we are no longer supporting so call "basic" boot but only "trusted" (using TF-A) .. but this does not mean Secure.

"Trusted" boot chain allow security but not enable it by default.

Hope it's clearer.

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MWors.1
MWors.1Author
Associate II
Jan 11, 2021 7:30 AM UTC

@Community member​ 

Prior to this discussion, I attempted to flash a base_defconfig, signed by the STM32MP_SigningTool_CLI.exe to my DevKit. After attempting this flash, it seems the board can't be flashed back to the original settings. Below is the log when I try to use the flash tool to return to the previous working configuration:

PS C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin> ./STM32_Programmer_CLI.exe -c port=usb1 -w FlashLayout_sdcard_stm32mp157a-dk1-trusted.tsv
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.5.0
 -------------------------------------------------------------------
 
 
 
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 001C002E3438511538333630
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MP1
Device type : MPU
Device CPU : Cortex-A7
 
 
Start Embedded Flashing service
 
 
 
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157a-dk1-serialboot.stm32
 File : tf-a-stm32mp157a-dk1-serialboot.stm32
 Size : 237896 Bytes
 Partition ID : 0x01
 
Download in Progress:
██████████████████████████████████████████████████ 100%
 
File download complete
Time elapsed during download operation: 00:00:00.503
 
RUNNING Program ...
 PartID: :0x01
Start operation done successfully at partition 0x01
 
Flashlayout Programming ...
██████████████████████████████████████████████████ 100%
Running Flashlayout Partition ...
Flashlayout partition started successfully
 
 
Memory Programming ...
Opening and parsing file: u-boot-stm32mp157a-dk1-trusted.stm32
 File : u-boot-stm32mp157a-dk1-trusted.stm32
 Size : 902798 Bytes
 Partition ID : 0x03
 
Download in Progress:
██████████████████████████████████████████████████ 100%
 
File download complete
Time elapsed during download operation: 00:00:01.002
 
RUNNING Program ...
 PartID: :0x03
 
reconnecting the device ...
 
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2000, @Name /STM32MP157AAC Rev.B,
SN : 001C002E3438511538333630
FW version : 0x0110
Device ID : 0x0500
Start operation done successfully at partition 0x03
Error:
 
Error: unable to get the associate alternate setting of partition ID: 0xf1
Error: please make sure that your alternate settings have string descriptors with the right format
Error: unable to upload data from virtual partition
Received PhaseID == 0xFF, system is going to reboot

Is there anyway to recover this board?

Olivier GALLIEN
ST Technical Moderator
Jan 11, 2021 8:18 AM UTC

Hi @MWors.1​ ,

Can you please share the UART console output during flash operation ?

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MWors.1
MWors.1Author
Associate II
Jan 11, 2021 8:33 AM UTC

Hi @Community member​ 

​ 

Oddly enough, once I connected the uUSB to capture the output via TeraTerm, the flash succeeded. I changed nothing except attaching my USB to CN11 and starting up TeraTerm. So.. apparently that was all I needed.. I'm not sure why that was required to flash the board in this state.

I've since removed the uUSB and tried to go back to my standard flashing procedure, and now that works as expected again.

Any clue what attaching the uUSB to the DK changed?

Olivier GALLIEN
ST Technical Moderator
Jan 11, 2021 8:56 AM UTC

Hi @MWors.1​ 

Good news.

This behavior remind me a quite old bug due to ST-Link firmware.

Can you check installed version and upgrade ?

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.