Skip to main content
Associate II
Mar 17, 2025 4:28 PM UTC
Question

Watchdog Panic Debugging

Hi,

on my STM32MP157C / kirkstone 5.15.145 i'm currently debugging an issue which ends up in a panic handled by OPTEE:

 

E/TC:0 Panic 'Watchdog' at ?:0

 

at least i can reproduce it quickly by causing traffic on SPI (connected to a BMA280 ).

 

 

...
spi_stm32 44009000.spi: stm32h7_spi_read_rxfifo: 0 bytes left (sr=0000100a)
spi_stm32 44009000.spi: disable controller
spi_stm32 44009000.spi: stm32_spi_can_dma: false
spi_stm32 44009000.spi: stm32_spi_can_dma: false
spi_stm32 44009000.spi: disable controller
spi_stm32 44009000.spi: cpol=0 cpha=0 lsb_first=0 cs_high=0
spi_stm32 44009000.spi: stm32_spi_can_dma: false
spi_stm32 44009000.spi: stm32_spi_can_dma: false
spi_stm32 44009000.spi: stm32_spi_can_dma: false
spi_stm32 44009000.spi: transfer communication mode set to 1
spi_stm32 44009000.spi: data frame of 8-bit, data packet of 1 data frames
spi_stm32 44009000.spi: speed set to 12500000Hz
spi_stm32 44009000.spi: transfer of 1 bytes (1 data frames)
spi_stm32 44009000.spi: dma disabled
spi_stm32 44009000.spi: enable controller
spi_stm32 44009000.spi: stm32h7_spi_write_txfifo: 0 bytes left
spi_stm32 44009000.spi: disable controller
spi_stm32 44009000.spi: stm32_spi_can_dma: false
spi_stm32 44009000.spi: transfer communication mode set to 2
spi_stm32 44009000.spi: data frame of 8-bit, data packet of 4 data frames
spi_stm32 44009000.spi: speed set to 12500000Hz
spi_stm32 44009000.spi: transfer of 6 bytes (6 data frames)
spi_stm32 44009000.spi: dma disabled
spi_stm32 44009000.spi: enable controller
spi_stm32 44009000.spi: stm32h7_spi_read_rxfifo: 2 bytes left (sr=00012002)
E/TC:0 Panic 'Watchdog' at ?:0

 


I configured to use IWDG2 in NS context:

 

// kernel DTS and TF-A DTS
&iwdg2{
	status = "okay";

	/* USER CODE BEGIN iwdg2 */
	timeout-sec = <32>;
	/* USER CODE END iwdg2 */
};

 



Of course it would be perfect to get hints for the SPI issue;-)  But my more generic question is: HOW can we get more details, e.g. a stack trace of the blocking situation. Can i somehow move the handling of the Watchdog into the non-secure context to be able to dump the stack?

 

This topic has been closed for replies.

3 replies

Christophe Guibout
ST Technical Moderator
Mar 18, 2025 8:41 AM UTC

Hello @SimK,

 

For this kind of issue, I would recommand to use GDB :  During the SPI use case, at a moment, you will notice that the console is frozen : It means the system is blocked somewhere, so the watchdog is not kicked anymore which will lead to a reboot is less than 32s. During this time, you can start debugging the software with GDB to know where the system is blocked.

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SimKAuthor
Associate II
Mar 18, 2025 12:39 PM UTC

Hi,

thanks, i will try to continue as you proposed.

In parallel i'm trying to rollback commits in the kernel because it's perfectly working with our old software based on dunfell / kernel 5.4.192

br, Simon

SimKAuthor
Associate II
Mar 24, 2025 7:23 AM UTC

Hi,

to keep you updated: wasn't necessary to debug.

the last log with SPI verbosity (which was not always on visible) led me to a bug in the ST SPI driver

stm32h7_spi_read_rxfifo: 2 bytes left (sr=00012002)

https://github.com/STMicroelectronics/linux/commit/d6ab414eb4e4ea2dce7b3d34974e752ce6e53099

SR_RXPLVL was not considered which leads to polling until stall detection.

if you also want to use kernel 5.15.145 and have SPI devices connected (which is not that unlikely) - get this patch.