Skip to main content
Visitor II
May 13, 2025 2:04 PM UTC
Question

Watchdog OPTEE Panic when stopping in u-boot

Hi,

I have enabled iwdg2 in tf-a, uboot (PV="v2023.10-stm32mp-r1") , optee (version 4.0.0-stm32mp) and linux kernel(ver. v6.6-stm32mp) device trees for STM32MP133F. iwdg is enabled in non-secure world only.

&iwdg2 {
status = "okay";

/* USER CODE BEGIN iwdg2 */
timeout-sec = <60>;
/* USER CODE END iwdg2 */
};



When stopping in u-boot there are 2 scenarios that manifest as watchdog caused reset.

1. First scenario is when the system is just stopped and inactive in u-boot.
2. Second scenario is when running mtest in u-boot. (mtest writes and reads to addresses from 0xc0000000 to 0xc4000000; excluding the end address) 

With op-tee watchdog reset there is Panic stack unwind:

E/TC:0 Panic 'Watchdog' at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/drivers/stm32_iwdg.c:228 <stm32_iwdg_it_handler> 

E/TC:0 TEE load address @ 0xce000000 

E/TC:0 Call stack: 

E/TC:0 0xce00a1d4 print_kernel_stack at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/arch/arm/kernel/unwind_arm32.c:109 

E/TC:0 0xce086f08 __do_panic at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/kernel/panic.c:88 

E/TC:0 0xce03902c stm32_iwdg_it_handler at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/drivers/stm32_iwdg.c:228 

E/TC:0 0xce0821ac interrupt_call_handlers at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/kernel/interrupt.c:91 

E/TC:0 0xce02e8d0 gic_native_itr_handler at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/drivers/gic.c:659 

E/TC:0 0xce02e900 interrupt_main_handler at /usr/src/debug/optee-os-stm32mp/4.0.0-stm32mp-r1/core/drivers/gic.c:670 

E/TC:0 0xce000388 vector_fiq_entry at tmp-glibc/work/mcm_ng-oe-linux-gnueabi/optee-os-stm32mp/4.0.0-stm32mp-r1/git/core/arch/arm/kernel/thread_optee_smc_a32.S:93 


And this is another example of watchdog reboot where the system is stopped in u-boot (debug traces are enabled with additional watchdog reset debug trace added).

16:54:45:688 -> stm32mp-wdt watchdog@5a002000: IWDG reset
16:54:46:688 -> stm32mp-wdt watchdog@5a002000: IWDG reset
16:54:47:688 -> stm32mp-wdt watchdog@5a002000: IWDG reset
16:54:48:688 -> stm32mp-wdt watchdog@5a002000: IWDG reset
...
...
17:19:47:718 -> stm32mp-wdt watchdog@5a002000: IWDG reset
17:19:48:718 -> stm32mp-wdt watchdog@5a002000: IWDG reset
17:21:16:953 -> NOTICE: CPU: STM32MP133F Rev.Y
17:21:16:956 -> NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06
17:21:16:978 -> NOTICE: Reset reason (0x204):
17:21:16:981 -> INFO: IWDG2 Reset (rst_iwdg2)


After some time the u-boot stops refreshing watchdog and there is subsequent reset.

Can you please suggest how to debug this issue and if there is something wrong with described iwdg2 configuration?

This topic has been closed for replies.